Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 Hi

   

Im trying to   test an82072 but it is not stable in USB data transfer.

   

mostly sending the data from PC to psoc kit (CY8Ckit-001 with PSOC3 prod.) so can change the DC and not the LED state.

   

from time to time the opposite happens - can send but cant receive (ADC value and button state).

   

I'm using windows8 (tried on win7 same problem) and i also tried to update the project component but with no success.

   

I also tried to change the USB cable.

   

 

   

 

   

need help ASAP.

   

 

   

thanks Guy

0 Likes
3 Replies
Anonymous
Not applicable
        Hi guyf   
Which archive did you use?   
AN82072(PSoC Creator 2.1 SP1) or   
AN82072_Archive(PSoC Creator 2.1_2.0) ?   
0 Likes
Anonymous
Not applicable

Im using AN82072(PSoC Creator 2.1 SP1) and my board has psoc 3 prod.

0 Likes
Anonymous
Not applicable
        Hi guyf   
I had been done AN project   
USB connection was established   
Every data had transmitted   
PC to device: PWM, LED sw   
Device to PC: AD data, SW status   
All seems working as well   
   
But, I have to mention Host application behavior   
It is working well itself but   
This program have affected on other USB connection   
   
When I have been turn on this program,   
another USB device has disfunctional   
This is very strange   
We might have to check the Host application.   
0 Likes