Announcements

Ever wondered how you could shape the future in collaboration with others? Join us at OktoberTech Asia Pacific and get inspired. Click here to sign up FREE of charge.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable
0 Likes
5 Replies
Bob_Marlowe
Level 10
First like given 50 questions asked 10 questions asked
Level 10

Welcome in the forum!

   

Easiest solution without any formatting is to use ftoa().

   

More complex but much more universal is sprintf(). Formatting specifiers here: publications.gbdirect.co.uk/c_book/chapter9/formatted_io.html

   

Internal enabling see here : www.cypress.com/

   

So increase stack and address the linker addition.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
100 sign-ins 5 likes given 1000 replies posted
Level 9

Usefull formatting discussion, attached.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 First, just want say sorry because I created the thread but couldnt type anything on the post due to some weird error on my web browser (Google Chrome).Really appreciate your reply. 

   
     I'm new to community and was struggling with the sprinf() whole day. I'm writing a code to implement a stopwatch on PSoC 5LP kit. I used a timer block to count the time between the Start and Stop buttons are pressed. Stopwatch is the Timer block. the code is roughly like below:   
   
        
   
    
     #include "stdio.h"    
    
     #include <project.h>    
    
     #define TRUE 1    
    
     #define FALSE 0    
    
     #define STOPWATCH_FREQ 10000    
    
     asm (".global _printf_float"); //adds ~8000 bytes to the program    
    
          
    
     int main()    
    
     {    
    
         //Set to TRUE if the stopwatch has started, else FALSE    
    
         uint8 started_b = FALSE;    
    
         //Temporary storage for status register    
    
         uint8 reg;    
    
         //Capture/counter read value    
    
         uint32 capture;    
    
         //Capture/counter converted to seconds    
    
         float seconds;    
    
         //Temporary string for sprintf to use    
    
         char tstr[16];    
    
         /* Place your initialization/startup code here (e.g. MyInst_Start()) */    
    
         SecondTimer_Start();    
    
         Stopwatch_Start();    
    
         Display_Start();    
    
         StopwatchStart_Read();    
    
         Display_Position(0, 0);    
    
         Display_PrintString("Stopped")      ;    
    
         /* CyGlobalIntEnable; */ /* Uncomment this line to enable global interrupts. */    
    
         for(;;)    
    
         {    
    
             if(!started_b)    
    
             {    
    
                 //If the stopwatch isn't known to have started yet,    
    
                 //see if the start button has been pressed. If it has    
    
                 //been pressed, the stopwatch has started.    
    
                 if(StopwatchStart_Read())    
    
                 {    
    
                     started_b = TRUE;    
    
                     Display_ClearDisplay();    
    
                     Display_Position(0, 0);    
    
                     Display_PrintString("Started")      ;    
    
                 }    
    
             }    
   
   
    
     //Else, check to see if the stopwatch has been stopped.    
    
                 reg = Stopwatch_ReadStatusRegister()      ;    
    
                 //If the stopwatch has been stopped, first read the capture    
    
                 if(reg & Stopwatch_STATUS_CAPTURE)    
    
                 {    
    
                     capture = Stopwatch_ReadCapture();    
    
                     started_b = FALSE;    
    
                 }    
    
                 //Else, just read the counter    
    
                 else    
    
                 {    
    
                     capture = Stopwatch_ReadCounter();    
    
                 }    
    
                 //Convert the capture/counter to seconds and print it    
    
                 capture = Stopwatch_ReadPeriod() - capture;    
    
                 if(capture != 0)    
    
                 {    
    
                     seconds = capture / (float)STOPWATCH_FREQ;    
    
                     Display_Position(1, 0);    
    
                     sprintf(tstr, "%1.4f", seconds);    
    
                     Display_PrintString(tstr);    
    
                 }    
    
                 //If the stopwatch has stopped, reset it    
    
                 if(!started_b)    
    
                 {    
    
                     StopwatchReset_Write(1);    
    
                     StopwatchStart_Read();    
    
                     Display_Position(0, 0);    
    
                     Display_PrintString("Stopped")      ;    
   
   
        
   
        
   
     For some reasons, the whole project seems to be working but the "tstr" is not displayed on the LCD. I can see the value of "seconds" and "capture" are updated as soon as I press Start and Stop buttons (SWStart, SWStop).   
   
     I tried to manually debug it by replacing the "seconds" by an integer and it works. So I suspect that the spintf function just doesnt like the float value.   
0 Likes
ETRO_SSN583
Level 9
100 sign-ins 5 likes given 1000 replies posted
Level 9

You have enabled the nano support in the library -

   

 

   

    

   

          

   

http://www.cypress.com/?id=4&rID=87354     nano library

   

 

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Hi Dana,

   

Yes I intentionally added another 8K of flash into my code so that it can handle printing or scanning floating point. 

   

The result is same when i adjust the linker files by following your link.

   

Thank you for your help. 

   

Cheers.

0 Likes