Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

I have to switch to Cypress microcontrollers, but I do not know which one to direct me to.
I would need a microcontroller with 2 QEI, 4 SPI, 3 UART, 1 PWM and other meters.
I have to check a brushless motor, read one or two optical lines and read 3 adc.
which microcontroller can you recommend me?
best regards
Renato

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Best would be to use a PSoC5 which has got the most flexible I/O. Most of your interfaces are implemented using UDB resources which are plenty in PSoC5. operating frequency is up to 80MHz and you can have DMA.

Bob

View solution in original post

0 Likes
1 Reply
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Best would be to use a PSoC5 which has got the most flexible I/O. Most of your interfaces are implemented using UDB resources which are plenty in PSoC5. operating frequency is up to 80MHz and you can have DMA.

Bob

0 Likes