- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear community,
For my internship, I am interested in the maximum streaming rate when using a Delta Sigma ADC to read an input and output it using a VDAC. The actual signal that will be used for the control algorithm will also have to be filtered, which might introduce more delay than I am already experiencing. Moreover, the signal will be around 80 kHz.
During testing, I saw that a sinusoidal signal of 50 kHz already has quite some phase delay with respect to the original signal, when it is outputted to using a VDAC. Is this just the limit of the PSOC5 I am using? Or am I missing some things that might give me better performance? For reference on what I did, see the figures below (yellow is signal generator, blue is VDAC). Also, the project has been attached.
With kind regards,
Jim
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jim,
I see 4 clocks delay between the input and output. Somewhere in the DelSig-ADC's datasheet is mentioned that it needs 4 clocks to "prime".
Since the output (VDAC8) is already 8-bit, try to reduce ADC's resolution to 8-bit and rise sampling frequency to the max to improve frequency response.
Due to intgrating nature of DelSig-ADC, there will always be a delay. It's intended frequency domain is <20kHz. For 100+kHz domain consider using SAR-ADC.
/odissey1