Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Hi,

   

I'm having a problem getting the bootloader working when compiling under Creator 4.0.

   

The code has maths functions in and compiles with no bootloader.

   

As soon as I add the bootloadable errors are throw for each math function in the code.

   

 

   

I've tried adding m to the additional includes in the bootloader project to no avail.

0 Likes
2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Can you please post your complete project, so that we all can have a look at all of your settings. To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Embarrassingly it turned out to be the documented linker setting or additional includes

   

All goo and thanks for the reply MB

0 Likes