- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
we are currently working in the healthcare industry. We are using the CY8C5268AXI-LP047 microcontroller in our Product for the last 3 years. Now we are planning to add an OTA feature for the MCU.
Here is the detail of the system:
CY8C5268AXI-LP047 is connected with a Linux-based system through USB it received the hexadecimal commands from the Linux through USB and based on the commands it performs the serval task. We have a working code to upgrade(program) the firmware into MCU through USB with the help of PSOC(bootloader) but as our system is having a Linux operating system we are not able to flash the firmware remotely or over the air.
Please let us know if is there any way to flash the firmware code remotely/over the air on Ubuntu 16.04 LTS.