I have a big problem,
I can't open the serial monitor of mobaXterm anymore because the Kitprog is now recognised as a storage device and won't apear as a com port (but ik can still program it [led blinks when updating program]).
Can someone help me fix this????
Solved! Go to Solution.
Hello.
This is well documented in Kitprog manual.
Plug Kitprog into USB and power it up. The Amber LED is OFF when in Mass Programming Mode. Now, press and release Kitprog mode switch within 2 seconds. The Amber LED should be ON solid indicating it's in programming/debugging and UART mode.
Hello.
This is well documented in Kitprog manual.
Plug Kitprog into USB and power it up. The Amber LED is OFF when in Mass Programming Mode. Now, press and release Kitprog mode switch within 2 seconds. The Amber LED should be ON solid indicating it's in programming/debugging and UART mode.