I' ve been trying to write the code for a 8 by 7 keypad using polling method . The problem is that I have all the coloumns connected to 4.7K external pull up resistors. And I cant able to find out which drive mode to be set for both cols. & rows. I have tried every possible combination. Pls suggest which should be used and also pls verify my code. The project is attached below.  

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I would suggest not to use external resistors (if that is possible), otherwise you have a voltage divider between the internal pullup resistor and the external. This will result in a voltage that is neither High nor Low.

   

Bob

   

 

   

PS: I've posted some time ago a solution for a 3x4 matrix keyboard for PSoC3 and PSoC5. Just for your understanding have a look at it (with PSoC Creator 2.0) Search for "matrix" here or in the PSoCDeveloper forum.

View solution in original post

0 Likes
2 Replies