- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Ive been looking at interfacing an lm35 to the PSOC 3, ive looked at the sample ADC single ended mode, Ive modified the output to convert the output from the adc to temperature as such: temp =(float)output*100/1023;
I am using the ADC in 10 bit mode, I want a float output.
Problem is, that the output is the temperature but still in hex, so the room temperature is currently 25c but it comes up as 19H which is correct but not ideal.
Ive looked at a few topics from here:
This one: http://www.cypress.com/forum/known-problems-and-solutions/problem-whit-psoc1-adcinc-and-lm35
and this one: www.cypress.com/forum/psoc-1-device-programming/decode-hex-dec
Ive tried implementing what Bob has suggested from the second topic, but the compiler doesnt like that there is no ANSI function prototype for this fuction: csprintf
Ive included the stdio.h library file too, anything (probably obvious) I am missing?
thanks
Kind regards
Solved! Go to Solution.
- Labels:
-
PSoC 3
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Converting a hex to ASCII string is done with
sprintf(Buffer,FormatString,HexNumber). Probably the preceding "c" in the post you refer to was a simple typo.
Bob
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
Converting a hex to ASCII string is done with
sprintf(Buffer,FormatString,HexNumber). Probably the preceding "c" in the post you refer to was a simple typo.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Whoops... That's exactly what was wrong, the C was a typo indeed.
Thanks Bob,
Im sending it to a 16X2 LCD and the 9 for the Buffer is too many decimal places, Ive reduced the size of Buffer to 5 and its plenty,
However I notcied that when written to the LCD there is like two pipe symbols occupying a segment at the end of the temperature readout. It shows this whether the length of buffer is 5 or 9.
Im using LCD_PrintString(Buffer); to dusplay the result called 'Buffer' on the LCD
Any ideas?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
When you upload your workspace bundle I'll have a look at.To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.
Bob
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
Your LCD update frequency is quite too high. You get 10ksps and every time a sample is ready you print it. I would suggest you to insert a CyDelay(250) into your main-loop. Good wil be to clear the display (using spaces) before writing a new value.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Bob,
I inserted the delay, the transition on the LCD is much better.
Ive also added a LCDprint string(" ");
after printing the temperature although i still see the double pipe after the temperature.
thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Increase your Buffer[5] to [20]
Bob