- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I tried to use emWin5.46 to work with QVGA 2.2 TFT SPI 240x320 (ILI9341)
Color, coordinates, orientation do not match ...
The result you can see in the photo.
Any ideas, tips.
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Everything turned out to be simple:
It is noticeable that the problem appears when working with a large number of data.
I had to rewrite the function void TFT_SendArray (unsigned char * Data, int byteCount); in the LCD_ILI9341.c file
I used the function void SPIM_PutArray (const uint8 / uint16 buffer [], uint8 byteCount)
uint8 byteCount is a problem, it is not enough for emWin.
I just changed it to int.
It seems everything worked as it should.
Thanks for the help.
Eugene
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I tried your project and noticed that there are at least two problems
(1) In GUI_Init() a window command which limit the drawing area has used to
limit the drawing area to the upper half.
(2) TFT_orientation is wrong.
So for a quick fix for (2) is adding "TFT_SetOrientation(1) in MainTak()
like below, then at least we can read the letters.
========================
void MainTask(void) {
TFT_SetOrientation(1) ; // <----- here
GUI_Init();
TFT_SetOrientation(1) ; // <--- here again
GUI_SetBkColor(GUI_BLACK);
GUI_SetColor(GUI_WHITE);
GUI_Clear();
GUI_SetColor(GUI_WHITE);
GUI_SetFont(&GUI_Font24_ASCII);
GUI_DispStringHCenterAt("COLOR_DemoLUT - Sample", 160, 5);
_DemoLUT();
}
========================
But to fix the problem (1) you have to go and fix the library, since all is done in GUI_Init().
moto
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
Thanks.
Now I am trying to learn emWin5.46, in particular FlexColor and SPI.
I'm trying to figure out how to use emWin settings for FlexColor.
for example DISPLAY_ORIENTATION (....) and etc, but I see no effect
An example of a simple test:
int main(void)
{
CyGlobalIntEnable; /* Enable global interrupts. */
SPIM_Start();
TFT_SetOrientation(1) ;
GUI_Init();
TFT_SetOrientation(1) ;
GUI_Clear();
GUI_SetFont(&GUI_Font32_ASCII);
GUI_DispStringHCenterAt("Hello world", 0, 0);
GUI_DrawRect(50,50,200,100);
for(;;)
{
GUI_Delay(200);
}
}/* [] END OF FILE */
Result:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I found another source of problem,
which is that in the project the TFT driver was not get reset.
So I added another GPIO output and reset the TFT before starting initialization.
Meantime, although I tried to check LCD_ILI9341.c,
it seems that there is/are something flipping the TFT rotation inside GUI_Init(),
which is a black box library function.
So I still need to have TFT_SetOrientation(1) before and after GUI_Init().
part of main() in main.c
========================
int main(void)
{
CyGlobalIntEnable; /* Enable global interrupts. */
SPIM_Start();
TFT_BL_Write(0) ; /* Turn Backlight off */
TFT_nRESET_Write(0) ; /* reset TFT */
CyDelay(1000) ;
TFT_nRESET_Write(1) ; /* release reset */
TFT_SetOrientation(1) ;
GUI_Init();
TFT_SetOrientation(1) ;
GUI_Clear();
TFT_BL_Write(1) ; /* Turn Backlight on */
MainTask() ;
========================
MainTask() in header01.h
========================
void MainTask(void) {
GUI_SetBkColor(GUI_BLACK);
GUI_SetColor(GUI_WHITE);
GUI_Clear();
GUI_SetColor(GUI_WHITE);
GUI_SetFont(&GUI_Font24_ASCII);
GUI_DispStringHCenterAt("COLOR_DemoLUT - Sample", 160, 5);
_DemoLUT();
}
========================
Anyway after these struggles my modified project seems to do what was expected initially.
So, I hope that rest is you work!
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
DrawRect, DrawString functions seem to be working,
but some adjustment for color would be required.
Please refer to the manual of emWin for details.
====================
TFT_BL_Write(0) ; /* Turn Backlight off */
TFT_nRESET_Write(0) ; /* reset TFT */
CyDelay(1000) ;
TFT_nRESET_Write(1) ; /* release reset */
TFT_SetOrientation(1) ;
GUI_Init();
TFT_SetOrientation(1) ;
GUI_Clear();
TFT_BL_Write(1) ; /* Turn Backlight on */
GUI_SetFont(&GUI_Font32_ASCII);
GUI_DispStringHCenterAt("Hello world", 160, 0);
GUI_DrawRect(50,50,100,100);
GUI_SetColor(GUI_BLACK) ;
GUI_DrawRect(180, 150, 230, 200) ;
GUI_SetBkColor(GUI_WHITE) ;
GUI_DispStringAt("Here you go!", 10, 130) ;
for(;;) {
GUI_Delay(200);
}
====================
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you, I will add a reset later.
I see that the colors are inverted.
Temporary change in the LCD_ILI9341.C file
// Display Function Control
TFT_SendCMD (0xB6);
TFT_WriteData (0x08); // 0x0A
TFT_WriteData (0x82); // 02 A2
---------------------------------
It seems yes - is there a problem with initialization (GUI_Init () ??)
I do not see a complete screen ( only half of the screen)
and I can’t draw a rectangle with a side of more than 128
int main(void)
{
.......
GUI_Clear(); // MainTask();
TFT_SetOrientation(1);
GUI_SetFont(&GUI_Font32_ASCII);
GUI_SetBkColor(GUI_YELLOW); GUI_SetColor(GUI_RED);
for(data=0;data<240;data++) {GUI_DrawLine(0,0,320,data); }
for(data=0;data<320;data++) {GUI_DrawLine(0,0,data,240); }
GUI_DrawRoundedRect(5,10,155,100,10);
GUI_SetColor(GUI_BLUE);
GUI_ClearRect(0,0,320,240);// only half of the screen
GUI_DispStringAt("Hello world",0,0);
GUI_DrawRect(50,50,200,100);
..................
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
> It seems yes - is there a problem with initialization (GUI_Init () ??)
I added a UART and dumped SPI transaction, GUI_Init() is sending following command
after calling TFT_Init(orient) ;
==================
TFT_Init_Done This is the end part of TFT_Init()
TFT_SendCmd(0x00) No Operation
TFT_SendCmd(0x36) Memory Access Control
TFT_WriteData(0xA0) 1010_0000 MY=1, MX=0, MV=1, ML=0, BGR=0, MH=0 <--- This line is causing our head ache!
TFT_SendCmd(0x00) No Operation // following two blocks are specifying the display size, seems to be ok
TFT_SendCmd(0x2A) Column Address Set
TFT_WriteData(0x00) SC[15:8] = 0x00 SC = 0x0000
TFT_WriteData(0x00) SC[7:0] = 0x00
TFT_WriteData(0x01) EC[15:0] = 0x01 EC = 0x013F = 319
TFT_WriteData(0x3F) EC[7:0] = 0x3F
TFT_SendCmd(0x00) No Operation
TFT_SendCmd(0x2B) Page Address Set
TFT_WriteData(0x00) SP[15:8] = 0x00
TFT_WriteData(0x00) SP[7:0] = 0x00
TFT_WriteData(0x00) EP[15:8] = 0x00
TFT_WriteData(0xEF) EP[7:0] = 0xEF = 239
TFT_SendCmd(0x00) No Operation
TFT_SendCmd(0x2C) Memory Write
==================
> I do not see a complete screen ( only half of the screen)
> and I can’t draw a rectangle with a side of more than 128
I also encountered this problem, but after implementing nRESET sequence
it was solved. So I recommend you to connect a GPIO to the reset pin and
assert reset, wait a while (I'm waiting 1sec, probably too much), then de-assert reset.
Anyway, we are getting close, I hope.
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
With your modification, my color bar now looks ok.
With my system, which has reset-pin addition, your test routine shows up like below
/*************************/
GUI_Clear(); // MainTask();
TFT_SetOrientation(1);
GUI_SetFont(&GUI_Font32_ASCII);
GUI_SetBkColor(GUI_YELLOW); GUI_SetColor(GUI_RED);
for(data=0;data<240;data++) {GUI_DrawLine(0,0,319,data); }
for(data=0;data<320;data++) {GUI_DrawLine(0,0,data,239); }
GUI_SetColor(GUI_BLACK) ;
GUI_DrawRoundedRect(5,10,155,100,10);
GUI_SetColor(GUI_BLUE);
GUI_ClearRect(0,0,319,239);// only half of the screen
GUI_DispStringAt("Hello world",0,0);
GUI_DrawRect(50,50,200,100);
GUI_DrawRect(200, 150, 250, 200) ;
while(1) ; /* stay here */
/*************************/
The library seems to have some problem with drawing loooong rectangle.
Probably poor implementation of drawing a long line.
The shorter rectangle shows up OK.
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for the help.
One more question:
Have you tried to read the display ID? ( datasheet 8.3.23. Read ID4 )
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Everything turned out to be simple:
It is noticeable that the problem appears when working with a large number of data.
I had to rewrite the function void TFT_SendArray (unsigned char * Data, int byteCount); in the LCD_ILI9341.c file
I used the function void SPIM_PutArray (const uint8 / uint16 buffer [], uint8 byteCount)
uint8 byteCount is a problem, it is not enough for emWin.
I just changed it to int.
It seems everything worked as it should.
Thanks for the help.
Eugene
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Congratulations, you made it!
> SPIM_PutArray (const uint8 / uint16 buffer [], uint8 byteCount)
But I think this is almost a bug of Cypress Component.
For nowaday applications uint8 for length seems to be too short.
Anyway, I'm glad that hearing you can proceed now!
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
pavloven,
What screen update rate you get with emWin?
/odissey1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The screen refresh rate is commensurate with projects without emWin.
A little later, I will report the time to execute the GUI_ClearRect somand (0,0,320,240);
or another?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
> One more question:
> Have you tried to read the display ID? ( datasheet 8.3.23. Read ID4 )
I tried some, but all data came back as 0x00,
ID1: 0x00 ID2: 0x00 ID3:0x00
ID4: 0x00, 0x00, 0x00, 0x00
according to the datasheet EXTC must be high, but from the schematic
I could get for my Adafruit ILI9341 module does not show the connection
around the ILI9341, so, currently I can not tell if my program is doing ok or not.
Note: For my board, CPOL needed to be 1
SPI Format CPHA = 0, CPOL = 1
Display Power Mode came back as 0x00, 0x00, 0x65
Display Pixel Format came back as 0x00, 0x00, 0x4E
Display Signal Mode came back as 0x00, 0x00, 0x02, 0xFF...
SPI Format CPHA = 1, CPOL = 1
Display Power Mode came back as 0x00, 0x00, 0xCA
Display Pixel Format came back as 0x00, 0x00, 0x9C
Display Signal Mode came back as 0x00, 0x00, 0x05, 0xFF...
Anyway, FYI
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
for PLL_OUT = 64MHz SPI Bit Rate = 32Mbps:
GUI_ClearRect (0,0,320,240) command execution time equals 56 mS
And so far I have not read a stack of anything from the display.