Anonymous
Not applicable
Apr 22, 2010
02:38 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 22, 2010
02:38 AM
I need to run in two configurations:
base:
amplifier
short:
the same amplifier but analog column inputs 0 and 1 connected together
However configtbl.asm for both configurations misbehave properly.
short configuration modifies (unchange compared to base config) regs 70 to 77h but should 62h bit 7
during loading
when comes to unloading it modifies 75h to 05h (!!!!!)
Am I wrong?
Labels
- Labels:
-
PSoC 1
0 Replies