Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
gogolgoggly
Level 1
Level 1
5 replies posted First solution authored First reply posted

Hello, I like to control the amplitude of a clocksignal on a GPIO. I tried that with this layout:

gogolgoggly_0-1647964497633.png

The mux is in switch-mode.

0 Likes
1 Solution
gogolgoggly
Level 1
Level 1
5 replies posted First solution authored First reply posted

First of all thanks for your support. I've found a setup which works for me.

Iget a 2kHz signal and a 2khz signal with adjustable amplitude.

gogolgoggly_0-1648131883239.png

 

View solution in original post

0 Likes
12 Replies
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

What are the specifications of the Output signal you are trying to achieve?

If you provide these details, we may be able to help.

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

In your schematic, the AMux goes into Hi-Z mode on LOW, which becomes a sort of a sample-and-hold circuit. If  Pin_2 output is measured using 1MO/100pF scope probe, there likely be a steady signal. To receive modulated signal the AMux must be switched between the Pin_1 and 0V. To provide 0V to the AMux, it must be connected to external Pin,  connected to GND. 

InputModulator_01a_A.png

RodolfoGL
Employee
Employee
250 solutions authored 250 sign-ins 5 comments on KBA

If you are using PSoC 5LP, you can use the SIO pins and setup a programmable Vref with the VDAC. 

The SIO pins are only available in Port 12. You need to setup the Output drive level to Vref.

RodolfoGL_0-1648047131795.png

 

Top design screenshot:

RodolfoGL_1-1648047141233.png

 

0 Likes

Great notice, but i'm using a PSOC3.

0 Likes

This works with PSoC 3 too.

Better using one pin than 5 pins to do this...

I believe the minimum output voltage that can be achieved using SIO pins with Vref is approx 0.5V, not 0V

0 Likes

Note that the Vref is only used to define the VDD for the pin. The pin will work as a digital pin, when logic is low, drives 0 V, when logic is high, drives Vref.

0 Likes

I know it's been a while. But i'm also observing this behavior. I can control the amplizude down do ~0.5V. I don't get the reason why.

0 Likes
gogolgoggly
Level 1
Level 1
5 replies posted First solution authored First reply posted

First of all thanks for your support. I've found a setup which works for me.

Iget a 2kHz signal and a 2khz signal with adjustable amplitude.

gogolgoggly_0-1648131883239.png

 

0 Likes

,

I'm glad you have a solution.

You might want to turn on the "Buffered output".  The VDAC8 output is normally a medium impedance. Turning on "Buffered output" will place an opamp in Follower mode (1:1 gain) and provide a much lower impedance. 

A medium impedance output can be influenced by loading.   Less so with a low impedance.

Len
"Engineering is an Art. The Art of Compromise."
0 Likes

hogolgoggily,

Please notice a Sync component on the schematic. It removes Setup Time Violation between the 2kHh clock and the BUS_CLOCK

0 Likes

Thanks for the tip.

0 Likes