Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
alro_2373731
Level 1
Level 1

I am reading the CyResetStatus and it appears to stay after reading it,  should I manually set it to 0 after reading?

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The status information will get updated at the next reset, whichever the cause might be.

Bob

View solution in original post

0 Likes
2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The status information will get updated at the next reset, whichever the cause might be.

Bob

0 Likes

Ref: PSoC 5LP

I think you are confusing CyResetStatus, a RAM variable, and RESET_SR0, a hardware register. Reading the RAM variable will not result in it being reset.

Reading RESET_SR0 directly is supposed to result in it clearing, but maybe or maybe not the 2 upper bits? The documentation is hopelessly contradictory.

I think part of the reason for confusion here is that Cypress documents the physical hardware separately from the firmware that uses it. At the hardware level, RESET_SR0 supposedly clears when read. Except those upper 2 bits, which may not. Or maybe they do.

But RESET_SR0 is read by firmware during the boot process, and the value is supposed to be stored (via an intermediate transfer to CYREG_PHUB_CFGMEM23_CFG1), so the firmware that you write never has access to the value of the register before it is cleared - only a copy of it. Which may or may not be further manipulated by the boot firmware.

See Cm3Start.c

For unknown reasons, my firmware configuration (#defines) is such that the intermediate transfer never occurs, to the CyResetStatus value is not meaningful.

My attempts at getting Cypress to address this have been met with very loud silence.

0 Likes