PSoC™ 5, 3 & 1 Forum Discussions
PSoC™ 5, 3 & 1
Hi, In my project,i use EEPROM.I have no problem in writing and reading data from EEPROM,but while writing EEPROM the interrupts are distur...
Show More
Hi,
In my project,i use EEPROM.I have no problem in writing and reading data from EEPROM,but while writing EEPROM the interrupts are disturbed. My project needs continuous interrupt service. How can i rectify this problem....... Show Less
In my project,i use EEPROM.I have no problem in writing and reading data from EEPROM,but while writing EEPROM the interrupts are disturbed. My project needs continuous interrupt service. How can i rectify this problem....... Show Less
PSoC™ 5, 3 & 1
Hi All, I have spent the last 1 1/2 hours trying to read the pinouts in the CyFi101 training course but I cannot read 3 or 4 of them no...
Show More
Hi All,
I have spent the last 1 1/2 hours trying to read the pinouts in the CyFi101 training course but I cannot read 3 or 4 of them no matter what I try.
Does anyone have the pinouts working and could you please post a copy of them here so I can finish the course.
Thanks,
Tom Show Less
I have spent the last 1 1/2 hours trying to read the pinouts in the CyFi101 training course but I cannot read 3 or 4 of them no matter what I try.
Does anyone have the pinouts working and could you please post a copy of them here so I can finish the course.
Thanks,
Tom Show Less
PSoC™ 5, 3 & 1
I am working on a project with CYWUSB6934, now I have to write a FCC firmware about it, but I did not find any information or register setting...
Show More
I am working on a project with CYWUSB6934, now I have to write a FCC firmware about it, but I did not find any information or register settings about FCC on CYWUSB6934 datasheet, could any Cypress guys help me? more details will be better, thanks a lot
Show Less
PSoC™ 5, 3 & 1
Hi, I am wondering if I can use capsense if it is not located on the same pc board. For instance if I have a keypad that is external to...
Show More
Hi,
I am wondering if I can use capsense if it is not located on the same pc board. For instance if I have a keypad that is external to the main pc board that contains the capsense ic, can I just run the capsense wires to my keypad buttons only? Will it work if the capsense chip is not directly mounted on the keypad?
Does anyone have any examples they can show or discuss?
Thanks in advance. Show Less
I am wondering if I can use capsense if it is not located on the same pc board. For instance if I have a keypad that is external to the main pc board that contains the capsense ic, can I just run the capsense wires to my keypad buttons only? Will it work if the capsense chip is not directly mounted on the keypad?
Does anyone have any examples they can show or discuss?
Thanks in advance. Show Less
PSoC™ 5, 3 & 1
Hi, I am hoping someone can direct me in the right direction. I am looking to develop a control system that will perform the fol...
Show More
Hi,
I am hoping someone can direct me in the right direction.
I am looking to develop a control system that will perform the following functions and utilize the following features. Any help, in guiding me toward the required modules and kits would be appreciated. This is a learning project for myself and thought I might as well develop something practical while I learn.
The system I want to design will monitor various water levels and controls various peripherals.
Water monitoring specifics will be: Temperature, PH Level, Oxygen Reduction Potential, Salinty, etc.....
Peripherals will be lighting, power switches, USB, wireless, etc....
Eventual functionality will include software to control the system that will allow for a programmed interface with the ability to monitor and log and report on captured data.
Thanks,
Tom Show Less
I am hoping someone can direct me in the right direction.
I am looking to develop a control system that will perform the following functions and utilize the following features. Any help, in guiding me toward the required modules and kits would be appreciated. This is a learning project for myself and thought I might as well develop something practical while I learn.
The system I want to design will monitor various water levels and controls various peripherals.
Water monitoring specifics will be: Temperature, PH Level, Oxygen Reduction Potential, Salinty, etc.....
Peripherals will be lighting, power switches, USB, wireless, etc....
Eventual functionality will include software to control the system that will allow for a programmed interface with the ability to monitor and log and report on captured data.
Thanks,
Tom Show Less
PSoC™ 5, 3 & 1
The CYRF7936 have a operational temperature range from 0 to 70 C. Will this limit the use in outdoor applications? Can it operate at lower tem...
Show More
The CYRF7936 have a operational temperature range from 0 to 70 C. Will this limit the use in outdoor applications? Can it operate at lower temperatures?
Also, can you buy a hardware module using the CYRF7936(where), similar to the wirelessUSB modules?
Thanks,
Robert Show Less
Also, can you buy a hardware module using the CYRF7936(where), similar to the wirelessUSB modules?
Thanks,
Robert Show Less
PSoC™ 5, 3 & 1
I am an final year student with an project of RF by using Psoc, what I do is a Heartrate monitoring by using telemetry, well I already got a h...
Show More
I am an final year student with an project of RF by using Psoc, what I do is a Heartrate monitoring by using telemetry, well I already got a hear rate strap(POLAR T31) to detect heart rate(transmitters are worn around the chest and generate a 5kHz magnetic pulse with each heart beat they detect. The transmitted magnetic signals are fairly weak, but typically have a range of over 3 feet)
My tutor suggest me to use one quadrant psoc cy3209 set as an transceiver,means receive the RF signal from strap and then transmit the signal for longer distance~and could use the orthe quadrant set as an orther receiver(Hardware simulation) and then dispaly the data on PC.
As I am not familar with the Psoc, I do not know whether this method will be work or not, and which step I should start with Psoc? Show Less
My tutor suggest me to use one quadrant psoc cy3209 set as an transceiver,means receive the RF signal from strap and then transmit the signal for longer distance~and could use the orthe quadrant set as an orther receiver(Hardware simulation) and then dispaly the data on PC.
As I am not familar with the Psoc, I do not know whether this method will be work or not, and which step I should start with Psoc? Show Less
PSoC™ 5, 3 & 1
Hi I have the kit CY3271-EXP1 but When I tried use the card Weather Station Borad is not working in the screen of SCD only show 06 points o...
Show More
Hi
I have the kit CY3271-EXP1 but When I tried use the card Weather Station Borad is not working in the screen of SCD only show 06 points of Scan and the leds Red & Green of RF Expansion Board not blinking only 6 times and after no more
Please let me know how I can resolve this problem Show Less
I have the kit CY3271-EXP1 but When I tried use the card Weather Station Borad is not working in the screen of SCD only show 06 points of Scan and the leds Red & Green of RF Expansion Board not blinking only 6 times and after no more
Please let me know how I can resolve this problem Show Less
PSoC™ 5, 3 & 1
Hello. Does Cyprus provide generic drivers for the Cy7C637 chip for sending and receiving data with a USB transceiver? If not, i...
Show More
Hello.
Does Cyprus provide generic drivers for the Cy7C637 chip for sending and receiving data with a USB transceiver?
If not, is there clear documentation available to develop this?
Many thanks! Show Less
Does Cyprus provide generic drivers for the Cy7C637 chip for sending and receiving data with a USB transceiver?
If not, is there clear documentation available to develop this?
Many thanks! Show Less
PSoC™ 5, 3 & 1
I'm looking at the possibility of using Cyfi for our products. We want to use this wireless technology for communication between a remo...
Show More
I'm looking at the possibility of using Cyfi for our products.
We want to use this wireless technology for communication between a remote controller and several Light dimmer.
With one remote controller you will be able to dim / change colours of several light dimmer. (select the device and change it according to your wishes)
Is it possible to use multiple remotes to controll all light dimmers?
Because you Bind a Hub (remote controller) with a node (light dimmer) my understanding is dat you can only controll the light dimmer with the remote which was used for binding.
Are there any solutions to use multiple remotes?
Are there any "Cyfi modules" available which can be plugged onto our pcb.
(just like you have the WUSB pre made modules)
This will save us a lot of design time. (we do not have to care about pcb layout)
If yes; are these modules available as samples?
Thanks, BR,
Jasper Show Less
We want to use this wireless technology for communication between a remote controller and several Light dimmer.
With one remote controller you will be able to dim / change colours of several light dimmer. (select the device and change it according to your wishes)
Is it possible to use multiple remotes to controll all light dimmers?
Because you Bind a Hub (remote controller) with a node (light dimmer) my understanding is dat you can only controll the light dimmer with the remote which was used for binding.
Are there any solutions to use multiple remotes?
Are there any "Cyfi modules" available which can be plugged onto our pcb.
(just like you have the WUSB pre made modules)
This will save us a lot of design time. (we do not have to care about pcb layout)
If yes; are these modules available as samples?
Thanks, BR,
Jasper Show Less