PSoC™ 5, 3 & 1 Forum Discussions
PSoC™ 5, 3 & 1
Hi, Is +4 dBm output power possible with internal amplifier on CYRF7936? I ask because all info in datasheet and such says it should be...
Show More
Hi,
Is +4 dBm output power possible with internal amplifier on CYRF7936? I ask because all info in datasheet and such says it should be but if you look in CyFi modules config file the max output power is limited to PA6 which is 0dBm both in hub and node. A clarification would be much appreciated.
Best Regards
/Marcus Show Less
Is +4 dBm output power possible with internal amplifier on CYRF7936? I ask because all info in datasheet and such says it should be but if you look in CyFi modules config file the max output power is limited to PA6 which is 0dBm both in hub and node. A clarification would be much appreciated.
Best Regards
/Marcus Show Less
PSoC™ 5, 3 & 1
Does anyone know where I can get a technical manual for the CYRF7936. The data sheet has a table on page 12 but there are no detailed d...
Show More
Does anyone know where I can get a technical manual for the CYRF7936.
The data sheet has a table on page 12 but there are no detailed descriptions of the registers.
Show Less
The data sheet has a table on page 12 but there are no detailed descriptions of the registers.
Show Less
PSoC™ 5, 3 & 1
I'm wondering if it is possible to export data to a text file continuously without having to click export. I'm trying to read the data ...
Show More
I'm wondering if it is possible to export data to a text file continuously without having to click export.
I'm trying to read the data in real-time and rather not have someone constantly clicking export.
Show Less
I'm trying to read the data in real-time and rather not have someone constantly clicking export.
Show Less
PSoC™ 5, 3 & 1
Hi, I would like to bind, receive the sensor data in real-time and unbind - all from my own application which is driven by a web applic...
Show More
Hi,
I would like to bind, receive the sensor data in real-time and unbind - all from my own application which is driven by a web application. Sensor Control Dashboard does not seem to provide enough flexibility to do these operations. How can I go about it? Is there an SDK or API that exposes core SCD functions?
Thanks,
-Yani Show Less
I would like to bind, receive the sensor data in real-time and unbind - all from my own application which is driven by a web application. Sensor Control Dashboard does not seem to provide enough flexibility to do these operations. How can I go about it? Is there an SDK or API that exposes core SCD functions?
Thanks,
-Yani Show Less
PSoC™ 5, 3 & 1
Hi All, i am new to this forum, i'm working on cypress controller for the past 2 months. Doubts: 1. In my firmware, I h...
Show More
Hi All,
i am new to this forum, i'm working on cypress controller for the past 2 months.
Doubts:
1. In my firmware, I have set the Enpoint(6) buffer size as 512. But, in Get Transfer Size API call (for respective Endpoints - 6) is returning size as 4096.
why it is happenning ? if my endpoint size is 512 why it is returning 4096.
Transfer Size should be same as the Endpoint Buffer Size. if not, tell me for what purpose trasnfer size is using...
Please clarify the same
2. By Default, Cypress speec is high speed. Can you tell me Cypress API which will set the speed?
3.i need the reponse time for XferData Function, it is taking more than 16ms for getting data from board (in HIGH Speed) ?
Please Clarify my doubt as soon as possible.
Thanks
Ram Show Less
i am new to this forum, i'm working on cypress controller for the past 2 months.
Doubts:
1. In my firmware, I have set the Enpoint(6) buffer size as 512. But, in Get Transfer Size API call (for respective Endpoints - 6) is returning size as 4096.
why it is happenning ? if my endpoint size is 512 why it is returning 4096.
Transfer Size should be same as the Endpoint Buffer Size. if not, tell me for what purpose trasnfer size is using...
Please clarify the same
2. By Default, Cypress speec is high speed. Can you tell me Cypress API which will set the speed?
3.i need the reponse time for XferData Function, it is taking more than 16ms for getting data from board (in HIGH Speed) ?
Please Clarify my doubt as soon as possible.
Thanks
Ram Show Less
PSoC™ 5, 3 & 1
Developing a slider for control of light levels. Did some evaluation on slider design. We wish to have end segments be used for off and max le...
Show More
Developing a slider for control of light levels. Did some evaluation on slider design. We wish to have end segments be used for off and max level. I believe extending the end segment sensor to be larger will better guarantee a touch to that segment will produce the end values from the slider resolution output. This way the finger is not making contact with next segment at all.
Can anyone confirm this concept?
Thanks Show Less
Can anyone confirm this concept?
Thanks Show Less
PSoC™ 5, 3 & 1
Hello! I need to write down massive from operative memory of the controller in flesh-memory. How it to make? Can give an example? I will be...
Show More
Hello!
I need to write down massive from operative memory of the controller in flesh-memory. How it to make? Can give an example? I will be very grateful for the help. Show Less
I need to write down massive from operative memory of the controller in flesh-memory. How it to make? Can give an example? I will be very grateful for the help. Show Less
PSoC™ 5, 3 & 1
Hi All, Power PSoC can be used to implement different DC to DC converter topologies for example Buck, Boost, Floating Buck and Buck-Boo...
Show More
Hi All,
Power PSoC can be used to implement different DC to DC converter topologies for example Buck, Boost, Floating Buck and Buck-Boost. The efficiency of power converter depends on many parameters like switching frequency, mode of operation (Continuous and Discontinuos), selection of external components (Inductor, Capacitor etc), Proper Layout etc.
We have mentioned minimum efficiency of 90% in Power PSoC datasheet and practically we have achieved upto 95%.
Please find the application note related to PCB guideline available on following link:
http://www.cypress.com/?rID=35361
Cheers,
Brijesh Show Less
Power PSoC can be used to implement different DC to DC converter topologies for example Buck, Boost, Floating Buck and Buck-Boost. The efficiency of power converter depends on many parameters like switching frequency, mode of operation (Continuous and Discontinuos), selection of external components (Inductor, Capacitor etc), Proper Layout etc.
We have mentioned minimum efficiency of 90% in Power PSoC datasheet and practically we have achieved upto 95%.
Please find the application note related to PCB guideline available on following link:
http://www.cypress.com/?rID=35361
Cheers,
Brijesh Show Less