PSoC™ 5, 3 & 1 Forum Discussions
Hello everbody,
i hope you can help me a little bit.
At the moment I am trying to program a PSoC 5 (CY8C5268LTI-LP030) with the CommandLineInterface.
Unfortunatey it isn´t working properly 😞
What have I done...
At the moment I am using this commands in a script:
OpenPort KitProg/0720063201324400 C:\Program Files (x86)\Cypress\Programmer
HEX_ReadFile "C:/HexFile/Testfile.hex"
SetAcquireMode "Reset"
SetProtocol 8
SetProtocolClock 152
SetProtocolConnector 0
SetPowerVoltage 5.0
//PowerOn
DAP_AcquireChip
PSoC3_EraseAll
PSoC3_ProgramRowFromHex 0x03 0 0
DAP_ReleaseChip
ClosePort
quit
Till the command "PSoC3_ProgramRowFromHex 0x03 0 0 " everything looks good. But while using this command I get following error message:
"PSoC3_ProgramRowFromHex 0x03 0 0
E
Timeout of SPC polling. Lost communication with chip (Status = 0x00)
PSoC3_ProgramRowFromHex 0x03 0 0 returned 80004005
80004005 OK"
And I am not sure how to fix it. I don´t know the problem... Is there anybody with an idea how to fix it?
Question 2:
Is there a command to program the whole hexfile without the rowId and arrayId? For example the command Program(). Unfortunately the UserGuid tells me it is only for PsoC1 😞
And is the arrayId 0x03 the correct id?
Many thanks in advance. I hope somebody can help me! 🙂
Ando some more informationen.
I am using a KitProg2 and the programming with PsocCreator oder PscoCProgrammer is working without any problems. So I guess there is no hardwareproblem.
We have an application, in which, two trans-receiver are paired with unique address, master quering the slave for it's presence, say every one second or so. If link is broken due to one of the device forming the pair move out of RF link range (150 ft. line of sight - outdoor, reduced inside the building) then alarm action is activated.
We want to know, is it posiible to have 300 or more such pair operating inside same building or an hall area of 3000 sq. ft., with out interfering with each other's operation.
Both Master and slave will be battery operated and carried by two different persons, accomping each other.
Please suggest practical solution and applicability of CyFi in above application
Regards
Vinay Dand
Mumbai
electrocentre@vsnl.com
Show Less
- « Previous
- Next »