PSoC™ 5, 3 & 1 Forum Discussions
Hello community,
I´m using a CY8C29466 to read some analog signals, communicate via UART and SPI and make a timer.
I´m using interrupt for the Uart´s, SPI and timer. Everithing work fine, until I enable the AD. If it execute the commands:
AD_14bits_Start(AD_14bits_HIGHPOWER);
AD_14bits_StartAD();
none of the interrupts work. Has someone experienced something like this? Could it be some configuration?
I would appreciate some help.
Regards,
Michel
Show LessI'm working with the BootLdrUSBFS module but I'm struggling to get the upgrader to work properly.
If I invoke the bootloader at the beginning of main.c, the upgrade does seem to transfer successfully however the changes don't stick.
If I invoke the bootloader after USB enumeration has occured I seem to end up in a hung state.
Is there some obvious things that I'm missing here?
Show LessI wrote the topic with wrong attached file that couldn't explain whole of my project.
so, i rewrite again here.
the problem is same.
Do not work PWMs with OP-AMPs
This time, I attach 4 pictures that could explain whole of my project.
maybe, a problem of the CY8C3866AXI-040.
maybe, a problem of my design.
Please solve this Problem.
Thank you.
Show LessI wrote topic with wrong attached file that can't explain whole of my project.
so, i rewrite topic hare.
Problem is same as before topic.
Do not work the PWM with Op-amps.
I attached 4 pictures that could explain whole of my project.
Please solve this problem.
Thank you.
Show LessI made a board using CY8C3866AXI-040
and i designed PWM like attached file.
when i use only PWM it is work perfectly.
but when i use a Opamp with the pwm, the pwm isn't work.
should i set something?
please solve this problem.
Thank you.
Show LessHello,
I am a newbie , I have downloaded the CY3663 development Kit and installed it. But I found that the firmware develop environment of cy7c67300 is gnu tools set, which I have not heard. There are several simple example in Cy3663 development kit, but I do not know which is the firmware program ,let alone modify it ,can you give me some help?thanks.
Show LessHello,
Is it really so that you can't more than one active debugging event at once in Psoc ICE (Psoc designer 5.0)?
Now I have watched the "Psoc Designer Module 3" debugging and there is instructed that one should but a switch as a first event. With that switch you can choose which event you would like to jump to.
Sure you can do this but this also means that only one active event at any time.
I have played with it a bit and realised that if you put two trivial events with breaks on with both, the another one won't work.
I am kind of missing more from the user interface here also. It would be nice to set write/read breakpoints at variables easily and not with this little bit hard to use event system.
Thanks
Show LessHi,
I have looked around in the cypress site but I wasn't able to find the MiniProg3 - cy8ckit-002 - programmer user Manual.
I need to know if it is able to program (via the Reset Mode) a +3,3V powered device - in the AN2014 they say that only ICE-cube can actually program a vdd=3.3V device. Is there a manual available?
Thank you
Show LessHi.
I'm using the PSoC3 first touch starter kit CY8CKIT-003.
I'm trying to use the VDAC8 to push out a chirp signal (a sine wave of linearly varying frequency from 38kHz to 42kHz). To get the values, I'm using a lookup table similar to the example on the online training video LAB 4 (the working man's oscilloscope)
The lookup table's inside an interrupt handler.
Question 1: The code provided with the training video doesn't work: My PSoC creator says that some of the code is outdated. Even if I update it, the code does not fully work. For some reason the program control shifts to the interrupt handler (I know this because I set a 'happy light' led to light up (and complement itself the next time the interrupt occurs) when an interrupt occurs) BUT it does not retrigger that interrupt some time later, as would be expected.
Question 2: Is there something I'm missing, like clearing an interrupt flag somewhere?
Show Less