PSoC™ 5, 3 & 1 Forum Discussions
sorry to post here but I found no other forum more pertinent.
I am developing a PSOC system with the Power Line Communication Module CY8CPLC10.
I checked the datasheet, but I found no suggested transformer for the signal path, except one that is obsolete.
So I googled around and found the Pulse Eng PE-65812 and PE-65612 transformers, that are suggested for Echelon applications and other digital audio applications.
I think that it should be ok, but I am not sure. Did someone tried it? and can someone suggest some part that is ok for this kind of application?
By The Way, I am using the CY8CPLC10 that is a simple i2c modem. Can it be used in conjunction with the CY8C27443-24SX microcontroller? I found no PLC module inside the PSoc Designer, but I think that it should be simply a matter of software library...
Thank you in advance!
Regards,
Federico Fuga
Show Less
I am running a C based application on PSoC Creator for PSoC3 based board.I applied three breakpoints to debug the code.In this process,when i stepped into the code at the third breakpoint using "step into" debug option,the control is swicthing to a disassembly code rather than the C-code instruction.Any help to solve this is appreciated.
Show LessI have one chip connected with address 04. I can't communicate with it via I2C although I am able to program it.
During I2C session response alwas is FF-
I conclude miniprog3 failed, because I't worked with several chips in the morning, but now it don't wiht neither of them.
ALso there is a strange device listing. Can someone try listing devices connected.
Miniprog3 device listing (using List button:
Devices list: 8bit 7bit
address: 0C 06
address: 0E 07
address: 1A 0D
address: 26 13
address: 32 19
address: 3E 1F
address: 4A 25
address: 56 2B
address: 62 31
address: 64 32
address: 70 38
address: 7C 3E
address: 7E 3F
address: 8A 45
address: 96 4B
address: A2 51
address: AE 57
address: BA 5D
address: BC 5E
address: CA 65
address: D6 6B
address: E2 71
address: EE 77
address: FA 7D
Can someone provide me a link to download CY8C55 family datasheet.The file(english) is damaged at the following link
http://www.cypress.com/?rID=37581
Show LessAre there already the winners for phase one? How many contestants submitted designs and when does phase two start? Do I get an eMail, if my design (named "MultiLogger") is not one of the top 100 designs for phase two?
Show LessThis BUG was reported 2 years ago. It seem very difficult to put brackets around directories that spaces would be interpreted as dir continuation.
Regards
robert
C:\Program Files\Cypress\PSoC Creator\1.0\PSoC Creator\bin\cyp3isrpatcher.exe "C:/Projects/PSOC/psoc3/PSoC 3 FirstTouch Starter Kit/1.0/Firmware/ProximitySense/ProximitySense.cydsn/DP8051_Keil_816/Release/ProximitySense.omf"
The application 'C:\Program' could not be started. Error: '%1 is not a valid Win32 application.
'
The command 'C:\Program Files\Cypress\PSoC Creator\1.0\PSoC Creator\bin\cyp3isrpatcher.exe' failed with exit code '2147483650'.
--------------- Build Failed: 02/04/2011 08:00:20 ---------------
This bug was reported 2 years ago.
Regards
robert
C:\Program Files\Cypress\PSoC Creator\1.0\PSoC Creator\bin\cyp3isrpatcher.exe "C:/Projects/PSOC/psoc3/PSoC 3 FirstTouch Starter Kit/1.0/Firmware/ProximitySense/ProximitySense.cydsn/DP8051_Keil_816/Release/ProximitySense.omf"
The application 'C:\Program' could not be started. Error: '%1 is not a valid Win32 application.
'
The command 'C:\Program Files\Cypress\PSoC Creator\1.0\PSoC Creator\bin\cyp3isrpatcher.exe' failed with exit code '2147483650'.
--------------- Build Failed: 02/04/2011 08:00:20 ---------------
I uploaded block diagram with abastract in Microsoft word .doc format. Is that acceptable?
SIr,
Thanks for your immediate reply . My design is in the need of two ports(pins) for the stepper motor operation. Basically I am trying to operate the stepper motor through the PSoc5, So can you please give me the information regarding the stepper motor ports on the kit or else any alternative solution in order to rotate the stepper motor using PSoc Kit.
Awaiting for our reply ,
Regards,
Narra
Show LessI have found the PWM user modules estimate the output period adding an Offset equal
to 1 clk cycle of your external clock.
Therefore the formula remains finally:
Tout= nºPERIOD*Tclk+1cycle_clk;
(Where nºPERIOD is the counter PERIOD, the number of clk input risng edges to calculate
the PWM output square wave period).
I have supposed it's due to a kind of precharge or setup time te PWM UM needs to charge again the values
in the counter or make the interrupts once the countdown is over.
I haven't find any statement about this in the PWM datasheet.
Anyone could confirm that theory or I'm wrong?
Thanks for all.