PSoC™ 5, 3 & 1 Forum Discussions
Now that the contestants have started receiving the Kits, feel free to share your experience and post the questions or doubts you encountered while working on the Kit.
Regards,
dasg
Show LessI know you have all been waiting; the kits have finally started shipping out so far about 90 percent of them so everyone should have them by the middle of next week.
If you don’t receive your kit let me know at Jeffrey.musante@cypress.com.
Good luck with your designs,
Jeff
Show LessThe message is:
SendI2CPacket() failed in CyMp3Service!
whenever I'm trying to send I2c packet through the brige rev 12 application.
What could it be?
Regards
Robert Seczkowski
Show LessDid you know that the PSoC 3 Boost Coverter lets you power PSoC from voltages as low as 0.5 Volt ? This feature is fully functional in the ES3 Silicon. This implies the chip using a single AA/ AAA battery or even a Solar cell.
-Udayan
Show Lessmy problem is:
How do I count the number of high-level output of a comparator zero-crossing?
I have to count how many zero-crossing exist in a second, therefore a counter must count for 1 second and give back the number of zero-crossing and put it in a global variable.
any idea?
thanks all!
Example 5 CapSense code, Page 151:
extern const uint8 LCD_Char_1_customFonts[];
should be:
extern const uint8 CYCODE LCD_Char_1_customFonts[];
in order to make the sample code link properly.
Show LessHi to all,...
I am working on my recent project , in that i am planning to replace video cable(VGA) between laptop and projector.....
so,...for that i am planning to use option 1) in that i want to use psoc3 and on board (CY8CKIT - 001) wireless module to transfer data..... i known that in laptop ,... setting adhoc network we can transmit some video data...and at receiver side (at projector without wireless facility),we can receive that data through PSOC kit....
so,..is it possible ??
and if i want to use wireless usb option 2) that how wireless usb can interface on CY8CKIT - 001 kit .... ?
guide me....
thanks.
Show LessI want to use boost converter to boost 5V out of Li-Ion battery and to let 4.2V battery voltage to drain down to 3V before recharge. What voltage level I set booster input voltage? Or do I need to regulate first battery voltage down to 3 volt and then boost it up to 5 volt?
Show LessWe're planning to use PSoC on a rocket as the flight computer and was wondering if there was anyone out there who has previous experience with using a PSoC to stabilize a rocket
Show Less