PSoC™ 5, 3 & 1 Forum Discussions
hi there,
actually i want an instrumentation amplifier for extracting sensor output do we have a instrumentation in psoc 3 or 5 or can we use pga (programmable gain amplifier) in differntial mode plz help
thank you
Show LessCypress released the new CY8CKIT-030 Development Kit for its PSoC® 3 architecture, along with a new version of its PSoC CreatorTM software tool! Get more info here!
Show LessHello,
I've got a cy3268 and I've programmed It correctly using the ice-cube. My problem is that when I try to debug using the ice-cube I get the message-window that says that the designer cannot connect to the ice. The message is exactly the one in the jpg that I have attached. I get the message after doing Debug->Connect from the menu of PSoCDesigner. The ice-cube is connected to the cy3268 in the same way It was when I downloaded the program in the board and in that occasion everything worked fine. I'm using PSoCDesigner 5.1 which I've recently downloaded.
Thanks for the help and have a nice day.
Trinca Claudio
Show Lessi tried to convert a analog signal to a digital one,using LED7SEG to show it ,but after adding the timer8 ,the system just don't work ,can you help?
this is my code ,thank you !
#include <m8c.h> // part specific constants and macros
#include "PSoCAPI.h" // PSoC API definitions for all User Modules
#pragma interrupt_handler timer
int TimerCount=0;
int iResult;
int i;
void main()
{
M8C_EnableGInt;
PGA_1_Start(PGA_1_MEDPOWER);
ADCINC12_1_Start(ADCINC12_1_MEDPOWER);
ADCINC12_1_GetSamples(0);
Timer8_1_Start();
Timer8_1_EnableInt();
LED7SEG_1_Start();
while(1)
{
if(ADCINC12_1_fIsDataAvailable()!=0)
{
iResult=ADCINC12_1_iGetData()+2048;
ADCINC12_1_ClearFlag();
iResult=iResult*5000.0/4096.0;
LED7SEG_1_DispInt(i,1,4);
if(iResult>2000)
{
PWM8_1_Start();
}
if(iResult<=2000)
{
PWM8_1_Stop();
}
}
}// Insert your main routine code here.
}
void timer()
{
TimerCount+=1;
if(TimerCount==128)
{
i=iResult;
TimerCount=0;
}
}
Hi,
I just bought 5 pieces of CY8CLED16P01-28PVXI and I solder it on my design circuit based on the CY3276 application notes. I implement the PLT user module in PSoC Designer and install on the chip. I use a simple transmitting code given by the example from PLC application notes. However, the chip won't transmit any data out from the FSK_OUT pin and so as the other four new pieces. The following attachment is my sample code. May I know what is the problem?
Thanks and your help is much appreciated.
Regards,
yx
Show LessThanks for your consideration.
-Mike
I wanna convert a analog signal(0-990mv) to a Digital signal, so i used a PGA (GAIN=4)and a ADCINC12,but the result is bigger than 4096,i am really confused,isn't the biggest output of ADCINC12 is 4096?
besides,what's the differences between AGND and VSS when i usibg them as the reference voltage of the PGA ?
thank you!
Show LessHello,
this post is the continuation of post "Ice cube recognition problem".
I have the cy3268 on which there is the cip whith the following marking:
CY8CLED04DOCD
1-56LTXI 0931
B 04 CHI
CYP 626613
The programming of the board with the ICE CUBE works fine, the problem is when I trie to do the debug. At this moment when I select "Debug->Connect" from the Designer I receive the message "Attached pod (00bf0022) is not compatible with the selected PSoC".
Looking around on the cypress web site I've found a similar post that goes like this:
Error Message: "Attached pod (000e1022) is not compatible with the selected PSoC" Last Updated: 11/30/2010 | ||
Question: I get an error message " Attached pod (000e1022) is not compatible with the selected PSoC" while using the new CY8C27002-24PVXI OCD part while debugging with PSoC Designer. This is the latest revision OCD part (B 05 datecode 1001). | ||
|
I am using PSD5.1 but is my problem anyway similar to this one?
Thank you very much and have a nice day.
Trinca Claudio
Show Less