PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
hi all,
can anybody please tell what is difference between psoc creator and designer to start with prototype designing in software whether i should go for creator or designer .....
thank you
Show LessOur group has purchased the evaluation board for the chip CYP15G0101DXB and we are unable to use the optical module. The information that came along with the eval board never explains how to use the optical module and we have tried several different setting combinations to make it work. Any insight would be benificial.
Show LessHi everyone,
I'm using the TX8 to send data through RS232. the data is received on Labview API. I have problems when the value is recieved there, because is like Labview no detect the terminator chart. As I read in the datasheet of TX8 the function TX8_PutCRL send an 0x0D ('\r') and 0x0A ('\n'). I put it this function after I send the value of the data.
Which terminator chart determine every data?
Thanks for your feedbacks!
Show LessLatest KB says, it's crashing because relitive path in a directory.
But in my case there is no additional relative path.
And it crashes at the very first moment of build process.
regards
rosaldo
Show LessHello everyone,
I am currently working on a project involving communication between two PSoC boards. Both of the boards will use an Artaflex AWP24S module. The purpose is to make the CY3209 act as a master and the PSoC 3 FirstTouch Starter Kit act as a slave. The CY8CKIT-003, slave, has an on-board +/- 2g accelerometer. The point is to fit the slave into a foam based football, throw it and measure g-force. After the reading has been done, it will transmit the value through WirelessUSB (using the AWP24S) to the main unit, the CY3209.
I have managed to program the master in a loopback and light up an led.
Do you know what module should I use in PSoC Creator for the slave unit, connect it to the master unit and send the information ?
I really need help on this one. Thank you.
Show LessI am using a graphics lcd (8080 interface) in my project. After finding it difficult to interface it with the psoc5 using the graphiclcdintf_v1_6 in creator I managed to inteface it by connecting it up using gpio pins in creator. I have set up my four control pins (nCS, nRD, nWR and AO) as digital outputs and connected them physically to the lcd. I have set up the 8 data pins as digital output/ digital inputs and connected to the lcd as well. I can write to the LCD perfectly - writing text and drawing some graphics. For routines that require reading, the problems begin. I cannot read the lcd memory! I suspect that I missed something in my pin setup. When i try setting up the data pins as bidirectional pins, I fail to even write to the lcd. When I set the pins as digital input and digital output I can write to the lcd but cannot read from it. Anyone with ideas- please help.
Show LessHello,
The real time clock has a 1 pulse per second (1 pps) feature that wakes up the device from sleep mode.
Is it possible to change this period? Say I wanted a 1/2 second pulse? This should be theoretically doable because my understanding is that the RTC XTAL drives a 13 bit counter internally. A modification of the counter's period should allow for this (perhaps via register write?)
Thanks,
Alex
Show Less