PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
I would like to us the SD flash as a data logger function. Does anyone know the maximum speed for writing? Also are there any other things to consider? Such as: Do I need pause statements after a write? I saw an app note that was using 24Mhz divided by 2. I am not sure how stable the data is at this speed. I would like to use the PSoC 5.
Thanks
Philip
Show LessHi all,
I am a beginner in Psoc .we are undertaking a project in which we are interfacing the Psoc ,which is monitoring a battery sytem , with LAN . For monitoring the battery we have decided to use the Psoc based Manager which is with the attached pdf. we have decided to use MOXA’s NE-4110S Ethernet Network Enabler Module with the Psoc for network interface. i want to know how to proceed with this with Psoc....
2) I heard Psoc creator is the tool for programming . so i want the Linux version(ubuntu 11.04) of Psoc creator
can anyone help?
i don know this is the correct place to post this?
if wrong correct me.
Thanks,
Kalli.s
Show LessGreatings Community!
I have faced with preaty strange fact.
I'm try`ing to create 10-chanel logic generator, based on counters whith two DMA chanels per each chanell.
first DMA refreshes Counter period (regulates perion lenght), second updates logic level (0/1).
the problem is :
some channels are reflected, some times are reflected and mirrored on another line.
(see pics below)
imageshack.us/g/13/newfile0.png/
each pic made with only one active Counter.
Can you tell me where am i wrong, or how to fix this problem?
I'm using CY8C3446AXI-099.
Design is attached.
Best Regards,
Alex C.
Show LessHi,
I've source code for specific usage of CY8C21223 chip for an application and circuit drawings.
How can I compile and program CY8C21223 chip? From the documentation, I undestand that PSoC Designer is needed and C compiler already included free. However, which kit do I need?
- CY8CKIT-001 PSoC® Development Kit - 249 USD,
- CY8CKIT-002 PSoC® MiniProg3 Program and Debug Kit - 89 USD
- CY8CKIT-014 PSoC® FirstTouch™ Starter Kit - 49 USD
Small modifications to C program may be needed, but not a major change or re-design is expected.
If I buy CY8CKIT-002, will it be enough?
Regards,
Murat
Show Lesshttp://www.cypress.com/?rID=2543
On this webpage, you can learn the software, kits along with the programming specs across PSoC 1, 3 and 5 families. The list of Cypress qualified production programming vendors is also posted here.
Show LessThe PSoC Programmer 3.13.1 release is a patch update provided support for the advanced release of PSoC Creator 2.0 and still supports PSoC Designer 5.1 SP2 releases.
This release of PSoC Programmer is available through the PSoC Programmer web page and through the CyInstaller Update Manager.
Please navigate to the Programmer Page for the installer and Release Notes.
www.cypress.com/go/psocprogrammer
The new features included with this release includes: update to support the Write Once Latch feature, new PSoC1 CapSense Device Support (CY8C20xx6L), etc.
Show LessCan anyone instruct me or point to the relevant document for changing the clock frequency supplied to the 8051 core in PSOC 3
Whats the maximum it can support??
Show LessCypress will have a big booth next week at the Embedded Systems Conference in Boston. The expo hall is open on Tuesday and Wednesday of next week (Sept 27th & 28th).
If you're in the area, stop by. I'll be working the booth both days. For more information, or to register (for free) visitwww.cypress.com/go/esc.
-Bobby
Cypress will have a big booth next week at the Embedded Systems Conference in Boston. The expo hall is open on Tuesday and Wednesday of next week (Sept 27th & 28th).
If you're in the area, stop by. I'll be working the booth both days.
-Bobby
Show Less