PSoC™ 5, 3 & 1 Forum Discussions
PSoC Designer 5.2 is released and is available through the PSoC Designer web page:
www.cypress.com/go/psocdesigner
PSoC Designer 5.2 is a minor release and will coexist with existing PSoC Designer 4.4, 5.0 and 5.1 installations.
The PSoC Designer 5.2 release has added the notable new features:
- Updated ImageCraft compiler
- Boot.tpl update to support custom code merge sections
- Support for CY8C20xx6L Device Family
- New SmartLED User Module
- CY8C20xx6L Devices Only
- New CSDe User Module
- CY8C20xx6L Devices Only
- Ovation ONS II LP Device Support
- Update to PowerPSoC SREG Sleep settings
- LINS user module support on new CY8C29xxx Automotive Devices
- New Wireless-NL User Module for all Encore II devices
- Update to SmartSense_EMC User Module
- Update to ADC10 and CSDADC User Modules
- New Device Package Support for CY7C638xx devices
- Co-existence with past PSoC Designer releases
We are also pleased to announce the PSoC Designer Youtube page. The Designer Team will post new videos announcing new features and walk users through example projects. Currently we have a tutorial walkthrough for “Your First PSoC Designer Project.” This video can be found directly on the Youtube channel or linked on the PSoC Designer landing age.
http://www.youtube.com/user/PSoCDesigner
http://www.cypress.com/go/psocdesigner
Thank you and Cypress appreciates your continued support of PSoC Designer.
Today I make the second Mini Prog3 bad when I was programming process,the VTARG and GND of Mini Prog3 is
Short-circuit. I want to konw why ?
Show LessUSB devices are so common today and it has pretty much become the standard of the day for data transfers and for many of the common applications. There is so much that can be done using USB. But how do you begin with USB? What is USB? What can I do with USB?
To learn about USB basics and probably more, visit the following blog post, Serial Ports are so 1990!
Is it possible to build a DQPSK transmitter and receiver in PSOC 5
Hey guys,
For the next revision of my custom PSoC3 board,one option I'm looking at is modifying existing kit design files available for download on the kits' webpage.I understand these are made in Cadence Allegro PCB editor(sorry for the bad naming,thats all I know about it).
My Questions are:
1.Is it legal to do so?
2.a.Apart from a copy of the software,what else would I need(no,not referring to tutorials)?.I'm referring to things like part libraries(like in eagle CAD..) etc..
2.b.Where do I obtain these pre-requisites?
Thanks.
Show LessThe PSoC Programmer 3.13.1 release is a patch update provided support for the advanced release of PSoC Creator 2.0 and still supports PSoC Designer 5.1 SP2 releases.
This release of PSoC Programmer is available through the PSoC Programmer web page and through the CyInstaller Update Manager.
Please navigate to the Programmer Page for the installer and Release Notes.
www.cypress.com/go/psocprogrammer
The new features included with this release includes: update to support the Write Once Latch feature, new PSoC1 CapSense Device Support (CY8C20xx6L), etc.
Show Less
I have a project using CY7C64215, now I need debug my code and program hex file. After reading the document of CY3210-PSoCEval1, I want to know:
Can I program CY7C64215 by this board and Miniprog?
Or, is there other economic way to program and debug CY7C64215?
Thanks.
Show LessHi folks,
Some of you might have been using CyUSB.dll and CyUSB.lib library for developing GUI to interact with Cypress USB devices including PSoC. It has now undergone plenty of changes and a new version with many improvements is now available for download here.
If you did not already know what Suite USB was, continue to read this App Note.
Show Lesshello:
How to configurate the DMA in my project? because i want to disable the
DMA transmission once it finishes transferring the desired data,and i set a
DMADone_flag in my main.c process,but when i build the process,i can't see
the DMADone_flag in project name.map document which disable my debug
processing?
Show Less