PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Hi all,
With PSoC Creator 2.0, the following Development Kit projects will fail.
CY8CKIT-050 - LowPowerDemo
CY8CKIT-001, CY8CKIT-010 - Ex4_USB_HID
To get installer package with updated example projects, please visit the product webpage.
Show LessI am trying to build code for the Psoc5 that uses the itoa function from stdlib.h.
I have the #include <stdlib.h> at the beginning of main.c but It is not being included and I am getting errors related to
undefined references to itoa. Do I need to explicitly set the include path in the build settings? and if so where would they be located.
Thanks
Show LessCan I run a GPIO pin as output, open drain, drive low and attach an external pullup to 5V while the system is running 3.3V? All VDDIO is 3.3V.
Show LessI intend to use an external RAM with a PSoc3 chip. I find EMI component is available in the standard component library.
And it has got ADDRESS , DATA and CONTROL type of I/Os. There are total five(5) I/Os are given without any detail .
The standard controls required for such interface are CE,OE and WR. However, to my surprise I coundn't find any hint
about the usages of the 5 Control pins in the component data sheet. So, when I sit with the hardware design I am not sure about the pin assignments. And I don't find any example on EMI as well. Also , I am not sure about the software implementation of the EMI. Can I get some help on this issue?
Regards.
A.R.Bhattacharya.
Show LessI used a RTC in PSoC3.
i defined a variable in main.c. i want to use the value of the variable in the RTC_INT.c . Let me know how to pass such a variable from main.c to RTC_INT.c file
regards
kavin
Show Lesshi developers,
i have a confusion in the basics. What is the function of a PSoC system sleep timer. how is it different from the watchdog timer. please help me out
Show LessHave you heard of Arduino ? I am sure you would have come across Arduino atleast once. Let me briefly tell you about Arduino. It is a platform which is considered to be the easiest embedded platform to work with. Programming an Arduino is child's play. The Arduino community makes what is called Arduino shield which can sit on top of any Arduino board and provide additional functionality such as XBEE, WIFI, Ethernet and so on.
A team at Michigan State University has now put together a PSoC5 board which will work with Arduino shield. The overall goal of this project is to have PSoC 5 be “Arduino-friendly”. In other words, one of the team at MSU is trying to have Arduino users purchase PSoC products. The overall goal of this project is to have a design that will prevent any technical difficulty when interacting Arduino shields with PSoC 5.
If you are interested in knowing more, http://www.egr.msu.edu/classes/ece480/capstone/fall11/group01/#about
Show Lesshi developers,
i was going through a wonderfully written application note AN32200 ( http://www.cypress.com/?docID=27337 ), on clocks and global resources. the description of VC3 clock source states( If i have understood it correctly) that VC3's every positive edge can be used as an interrupt. is that so.? if so how can we eneable or disable this interrupt in the designer IDE. i couldn't find any options like "VC3 interrupt enable/disable".
Show LessHi !
I'm extremely interested in the integeration to my current project a graphic LCD drived by a Solomon Systech SSD1926 controlleur, I would like to know then when the "CY8CKIT-032 Graphics LCD Interface Kit" will be released to custumer ?
Thank u in advance
Elias
Show LessHi !
I'm extremely interested in the integeration to my current project a graphic LCD drived by a Solomon Systech SSD1926 controlleur, I would like to know then when the "CY8CKIT-032 Graphics LCD Interface Kit" will be released to custumer ?
Thank u in advance
Show Less