PSoC™ 5, 3 & 1 Forum Discussions
Have you heard of Arduino ? I am sure you would have come across Arduino atleast once. Let me briefly tell you about Arduino. It is a platform which is considered to be the easiest embedded platform to work with. Programming an Arduino is child's play. The Arduino community makes what is called Arduino shield which can sit on top of any Arduino board and provide additional functionality such as XBEE, WIFI, Ethernet and so on.
A team at Michigan State University has now put together a PSoC5 board which will work with Arduino shield. The overall goal of this project is to have PSoC 5 be “Arduino-friendly”. In other words, one of the team at MSU is trying to have Arduino users purchase PSoC products. The overall goal of this project is to have a design that will prevent any technical difficulty when interacting Arduino shields with PSoC 5.
If you are interested in knowing more, http://www.egr.msu.edu/classes/ece480/capstone/fall11/group01/#about
Show LessOn module Counter_2_20 I get this warning:
" Error processing element 'register'. error at line 262: invalid address"
Should I be worried.
Thanks,
Phil
Show LessThis in spite of already having PSoc Programmer 3.10.1 Production installed.
The install path for 3.10.1 is C:\Program Files\Cypress\Programmer\3.10
I don't recall over-riding the default install path.
The install path for the FTRF drivers is C:\Program Files\Cypress\Programmer\3.10\drivers\ftrf
Sure don't want to back-level from 3.10.1 to 3.06 just to be able to install SCD 2.0.39 Show Less
Hello Everyone,
Here's an update on PSoC 1 kits available on our website-
CY3280-22x45 Universal CapSense Controller (UCC) kit is back on web
Your favorite CapSense Plus kit CY3280-22x45 is now available on the web for order. The CY3280-22x45 Universal CapSense Controller Board enables you to evaluate CapSense Plus capability of the CY8C22x45 device family. Both the kit project and the documentation have been updated to work with PSoC Designer 5.2. The kit includes:
- CY3280-22x45 Universal CapSense Controller Board
- CY3280-22x45 Universal CapSense Controller Board CD
- Quick Start Guide
- CY3240-I2USB Bridge
- CY3210 MiniProg1 Programmer
- USB Cable
Visit the landing page of this kit http://www.cypress.com/?rID=36805 for more information.
Got a question? Shoot an email to Sachin at sgup@cypress.com.
Regards,
Arvind
Show Less
Hello Everyone,
Frequency measurements are a common requirement of many applications.
AN2283 - PSoC® 1 Sensing - Measuring Frequency gives a good overview of the many methods that can be used along with their relative error in measurement.
The sample project in the above link, provides an example implementation that is accurate to 0.0016% (16 ppm).
Regards,
Arvind
Show LessHi,
This is for those who are facing an issue in installation of PSoC Designer 5.1 SP 2, where the installation hangs and does not complete. It issue has been faced by some users using Windows 7, Vista, XP. This is due to a Microsoft Installer Bug. This message is seen in the PSoC Designer 5.1 SP 2 download page ( http://www.cypress.com/?rID=41083) also.
So presently Cypress has provided a workaround by releasing an Emergency Patch. This can be downloaded at:
http://www.cypress.com/?rID=53393
Please use this only if you face problems with the normal version.
Regards,
Prem Sai
Show LessHey All,
Most of you might have read the appnote - AN73212 - Debugging with PSoC® 1 which gives a wealth of information about the debugging options that one has while working with PSoC and Designer.
I was also looking at one of the training modules (PSoC Designer Module 3: Debugging with PSoC) after a long time and found that it gave a real clear walkthrough of how each feature of the Debugger in Designer can be used. The examples probably cover most of the common fault scenarios. Even though the Designer version is old, it still covers the basic idea behind debugging with PSoC 1.
If you haven't watched this presentation so far, I highly recommend you do so today!
Only catch is that you can't view it online.. so please download the zip , extract and open the "player.html" in a browser.
Show Lesshow to use api change Uart’s Baud rate, stop bits, date bits