PSoC™ 5, 3 & 1 Forum Discussions
Hi all,
I managed to short Vin to ground while I had a 12v supply hooked up to the barrel plug on my board. No magic smoke came out of any of the chips (that I saw), but my board no longer works. When the j10 jumper is set to 3.3v the 3.3v regulator just above it gets rather hot (might burn me if I left it on). Also my VDDD has continuity to VSSD (ie, it's shorted to ground) when j10 is in any position (including not attached). I would geuss my 3.3v regulator was blown, but it's doing its job just fine (tested with a mulitmeter and I get 3.3v on the middle pin and the big tab). I also checked and confirmed that the caps in the power supply circuitry don't have continuity to gound. Any ideas on what to check next? or where I can buy another dev kit (everyone seems to be out of stock)?
Thanks,
Geoff
Show LessIs it possible to wake from sleep then:
1. Power up the ADC and OpAmps
2. Start a conversion
3. Power up the DFB
4. Pass the ADC sample to the DFB
5. Output the previous DFB result via I2C
6. Go back to sleep
All at 9ksps ?
I have severe power limitations!
Thanks,
Richard
Show LessI have warnings saying "Multiple call Start/Main Interupt/ISR" what is this warning saying and how to remove this.
I have this function called 'Start" which I am using in main as well as one of the interrupt routine. What has to be done to remove this warning
Show LessHi all,
There are many queries related to interfacing Character LCD (HD44780A) with PSoC 3/5 through different I/O pins from different ports, which is not possible through the Character LCD user module in PSoC Creator. Hence, i have attached a sample project which does this with detailed information.
Hope this helps!
Show LessDear all CDC members
I am designing and planning to implement SDR(software defined radio) on PSoC 001 Kit.
Please help me out for this project by posting sample projects and tips.
Show LessRead interesting app note on fsk modulation and demodulation
http://www.cypress.com/?rID=40985
Its worth reading, please have a look
Show LessAN61102 - PSoC® 3 and PSoC 5 - ADC Data Buffering Using DMA
Interesting appnote, guys have a look
http://www.cypress.com/?rID=44335
Show LessPlease read interesting App note on Analog signal chain calibration
AN68403 - PSoC® 3 / PSoC 5 - Analog Signal Chain Calibration
http://www.cypress.com/?rID=50320
Show Less