PSoC™ 5, 3 & 1 Forum Discussions
Hello! I'm new in the forum.I want to do a project programmer CY764713-128AXC.Unfortunately I did not find CY7C64713-128 AXC in to the library of the PCoC2 Creator! Help please!
Show LessHey Everybody
We are trying to use our first touch starter kit to make a self balancing robot. But it seems that the system won't let us use two custom build clock driven ISRs in the same time? Has anyone in here expirienced some similar problems, or does anyone know a solution?
Best Regards
Anders
Show LessHow many break points are possible in PSoC5?
SmartSense UM encapsulates CSD along with Auto-Tuning which was developed to simplify the user interface development cycle. It is easy to use and significantly reduces the design cycle time by eliminating the tuning process throughout the entire product development cycle, from prototype to mass production.
SmartSense tunes each CapSense sensor automatically at power up and then monitors and maintains optimum sensor performance during run time.
This technology adapts for manufacturing variation in PCBs, overlays, and noise generators such as LCD inverters, AC line noise, and switch-mode power supplies, and automatically tunes them out.
Show LessHello Friends,
If you did not notice the Home page of Cypress and missed out an opportunity to attend Virtual Conference of PSoC World, here is the link to register and enter the PSoC World conference.
You can register through the link
http://www.psocworld.com/register/
Hurry Up
Show LessIs there any indication of stack overflow in PSOC3/5
Hi guys,
ive been going through some sample projects available here, ive downloaded the fantastic psoc range finder app for my ct8c 29466 pxi. its pretty cool and is neat, very simple circuit which is great. I was thinking of wanting to modify the code to be used for tank liquid measurement, in a simplistic way rather than a distance display in cm's. I was thinking could it be modified to look at a water level and output 3 levels such as high, medium and low? it doesnt need to have the lcd either as i dont really need it. Ive done similar in college labs a few years ago with the psoc 3 but with temperature measurement, another thing i was thinking of was if the level suddenly drops as in more than an inch per minute to set an output high indictaing a leak?
Show Lesshi to all,
I am doing fan control using psoc 1 , but i am encountering a problem that when i am going connect 4 wire fan to pin , the voltage level at that pin is decreasing to 3 v but before connecting it shows 5v. why this reduction of voltage. and because of this fan not able to run. how to overcome this problem.
thanks
PRP
Show Less