PSoC™ 5, 3 & 1 Forum Discussions
2 hours ago, the drop down forum menus were working.
Now, there are no drop down menus. I have to keep going back to Infineon homepage in order to get to the forum I want.
I had to choose a Forum from this form, but the problem is with ALL the forum drop down menus. They're non-existent.
Running PC with Win10, MS Edge.
How about back tracking to the previous release of the forum software!!! It worked well enough to use. The current release is not usable.
Show Less
I need to develop a temperature sensing controller demo. This system will be installed in a vehicle which carries food products across locations. The temperature needs to be changed based on the food product i.e. different temperature for milk products, fruits etc. Can you suggest which kind of sensor will be suitable - Thermistor, Thermocouple or diode for this application?
Show LessHello, I'm trying to place 4 Quadrature Decoders, 4 Timers, 4 DACS and one UART in a CY8C5888-LP (using CY8CKIT-059). The UDB's Resources seem to be enough but build fails. Can anyone tell me where is the error? Thanks, Alfonso
Show LessCOMO OBTENGO LA DIRECCIÓN DE COUNTER_1 PARA CyDmaTdSetAddress
We are looking for information to code DMA functions to auto transfer data to and from SRAM and I2C Master and slave.
We were able to fit 3ea I2C Slaves and 3 I2C Masters along with 6 DMA modules into the CY8C5888LTI-LP097.
We need to setup the DMA channels to operate automatically and continuously to duplicate SRAM data from one 5888 to another 5888.
The data is 8-bits and we have 16 bytes to transfer. The number of SRAM to duplicate between MPU's may grow as the project grows.
I do not expect someone to code for us, just supply help understanding the DMA setup.
The datasheet is not clear or as clear as it could be.
Thank you for your assistance!
Show Less
Anybody know how to go to a bookmark in PSoC Creator? Have the ability to place bookmarks in files but can't seem to find a "go to next book mark" function.
Show Less