PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Hello,
I measure a current with a ADC_delsig and I want to send the measure 16bit with the SPI.
I have an SPI-SLAVE that communicates with a PIC18F97J60. The communcication works with 8-bit words, and I would also send in my frame a 16-bit words.
Thanks for your answer
Show LessHi, i making a aplication when i need to generate 3 independients wave forms, and controlate the type of this waves, the problem is that the unic mode that i find to change the wave type is in the wizzard but after i can´t modificate this. I hope that some body can say me if is this posible and how can i do it, becuase i searched in many archives .h and .c i can´t find it.
Show LessHi,
A button is pressed the rise a counter.I want to see the values of counter with 7 segment. I am using two seven segment multiplexing. Pressing button ones digit increasing but second digit(tens digit) is flashing a short period of time. Example, i want to count 25,26,27. 5,6,7 digits counting. But tens digits(2) flashing.CAn you see the program? What I'm doing wrong.
Show LessHello Friends,
Here is simple Baseline design for interfacing PIR with the PSoC 3/5. The PIR sensor available on the CY3236A PIRMOTION EVK was used(PIR Motion Sensor, 3POS Mfg by: Glolab Corp. Mfg part no: PIR325). Few modifications were done on the EVK and external components were used. The topdesign of the project has the schematic.
Description: The output of the PIR sensor is sent to two low pass filters one with a cutoff of 0.03Hz and other with a cutoff of 30Hz. The lower cutoff filter was used an a reference for the one end of delta Sigma ADC( configured in differential mode) anmd the output of higher cutoff given to the other end. The signal is suitable sampled and the digital value compared with the baseline and the Threshold to signal the detection.
I am attaching the project. The project is well commented.
Show LessHi all;
my project involves oversaw a photovoltaic Park using powerline communication specifying as hardware target integrated circuit CY8CPLC10 for data management, so I find a problem with the playback of data received via PLC indeed I can't Reset the RX Message Info array variable to clear the RX buffer for new messages by this registry (RX_Message_Info) is only read contrary to what shown in the note of application (AN52478) by cypress semiconductor?.
HI,
I am checking on example project and found the sample and hold example. The sample and hold component can use internal and exteranl as Vref, but I could not find any reference on why and when you should use the internal or external vref. Any idea where can I find the information?
Tks
Show Less