PSoC™ 5, 3 & 1 Forum Discussions
Dear PSoC Developers
I'm using USBFS component and I wrote program that I'm sending data from the PC to the PSoC 3 device (I configured as a HID device) and getting the same data back to the PC.
In the PC I'm using Libusb 1.0 library.
I was able to have the connection, but I cannot send more then 1 byte data, when I'm trying to send for example 2 bytes, it only sends the last 1 byte.
Is it possible to send more then 1 byte and how?
What should I change (maybe in HID descriptors)?
Thanks in advance
Gurgen
I had implement a Sleep Timer Module,
Interval was set to 8 milisec.
I was checking the interrupt period by using LED.
Interval was shows quite wrong time, around 16u.sec.
This interrupt type set to DERIVED.
When set it to RISING_EDGE, Interrupt never happend.
Tell me what's wrong.
I am controlling the Duty cycle of PWM output using the API given.. and its working fine, but the problem is with the amplitude.. i am expecting it arnd 3.3V (digital-3.3 & analo-5V).. but i am getting around 5V even after using a didital o/p pin.
What might be the reason behind this behavior?
Show LessHi all,
In my project I am using a temperature sensor (LM35) whose analog o/p is being signal conditioned by psoc. The psoc design is working fine as long as the i/p signal given to it is from a potentiometer on the board. When I am giving the Vout of the temperature sensor to the psoc emulator board, it is not working. The UART is displaying default garbage values. Can anyone tell me what to do? (I have also given a common ground for the sensor and psoc kit). One more thing is, I would like to transmit the data collected from the sensor wirelessly. Preferrably a zigbee module low power and high range. Any suggestions for modules that are compatible with psoc?
Show Less