PSoC™ 5, 3 & 1 Forum Discussions
This is the first for me.
As usually as, I'm doing LED test for after installing of PSoC.
Blinking LED the first part of main program.
Once lit, never again.
However, When select CPU Clock= SysClk/2
It began to blinking.
CPU Clock set to SysClk/1 again, It happen again
. Changing the chip was helpless.
What is happen in C29466?
How to do I?
Any suggestions? Show Less
Hello all,
I'm working on a circuit to move a mouth servo on a puppet, tracking live voice input. My current plan is to use the analog blocks to run the audio into a PGA, then through a band pass filter, and finally into an ADC. I have been using the filter wizard to set my parameters, but when I look at the output of the Band pass filter on the analog output buss, I see what looks like the signal chopped up, probably at the filter sample filter rate. Anyway, it looks like running the ADC on that signal would not give me a reliable voice amplitude. What should I do next, and what can I provide to the community for you to look at? Any suggestions for what I should set the parameters in the filter wizard to?
-Chuck
Show LessMy overall goal is to sample two signals at 30 ksps / signal (60 ksps total) and send the data via a wireless protocol such as bluetooth.
Current progress:
I'm able to sample one signal at 10 ksps using a 8-bit delta sig ADC. I'm able to send a few seconds of data at 10 ksps to the pc via UART. I may need to configure an external clock to get the required baud rate to match my hardware for 30 ksps.
My code currently sends one byte after each ADC conversion. I don't think that this is the best way, and I'm afraid it won't work well for 30-60 ksps.
Questions:
- Should I be using some kind of buffer to store data before sending it via UART?
- What's the best way to send streaming data via UART?
- Will I be able to two channel's worth of data (60 ksps) using UART without issue?
- Would you suggest that I use a serial-to-bluetooth module to make this design wireless? I've never used bluetooth, but the data rate seems to be ok for this application.
Just started using the psoc 5 and learning C programming a few days ago.
Figured I would share my frist project with everyone.
I know the coding is crude, but it was done just as a way to start using the psoc 5.
I have a few projects in mind for using it, and need to learn so much,
as there really is a lot going on in this chip.
any pointers as to using pwm for DDS in the 300KHz range and at 1Hz steps.
Also need to know how to get at the SC/CT blocks directly so I can make my own part.
So much to learn, so little time. 🙂
Anyways, I will post more as I learn more abot this chip and hope that other will find it useful.
Show Less