PSoC™ 5, 3 & 1 Forum Discussions
Hello,
I tried to run the Assembly Language Program but i am facing the error"The command 'Ax51.exe' failed with exit code '2'."
May i know how to rectify thiserror??
Show LessHi,
I am trying to implement a differential amplifier to convert an input signal range of 1-5V to 0-4 V. I tried it using 2 back to back PGAs with first stage (Gain=1,ref Vss) providing 1V ref to second stage(Gain=1) to which input signal of 1-5 volts is applied.But this did not work as expected.
Has anyone implemented it before?Please help me out.
Show LessTo pass constant char address is bad.
It seems a random data or random address was passing through
On 8C21434, that have 512Byte SRAM (Large memory model)
Enable paging option and
Treat const as RAM option not for help
Do you think what is wrong?
///////////////////////////////////////////////////////
static char buf[32];
void SubTest( const char* str )
{
//..cstrcpy( buf, "Test2" ); <--- this is good
... cstrcpy( buf, str ); <--- this is BAD
... UART_Send( buf ); <--- think like as LCD_PrString();
}
///////////////////////////////////////////////////////
void main()
{
... SubTest(" Test1 "); <--- call from here
}
///////////////////////////////////////////////////////
This was not occur on another device, ever
C24223 (small memory model) Show Less
Hi there!
Can anyone tell me please, which is the active state of "reset pin" on ant SPI componet ? I mean is "0" active or is "1" is active?
I puting a quote from de SPIM component pdf.
reset – Input
Resets the SPI state machine to the idle state. This throws out any data that was currently being transmitted or received but does not clear data from the FIFO that has already been received or is ready to be transmitted
Thank tou in advance.
Show LessIs there any code profiler for PSOC 1?
Thx
Hello Friends,
You are always in busy with Creator3.0, I presume.
Anyway, listen to my trouble of PSoC1.
UART signal that sent from PSoC1(8C24233) to (FTK3270/MTF Board 8C21434) was not received.
receive interrupt has not occur.
UART-Tx signal was lift up 1.7V (look wave1)
Sender is strong drive and receiver is High-Z input.
Even if resistive pull-down and pre-buffered by DigBuf
was not for help it.
For an experiment, No load output (look wave2)
It seems properly.
Any suggestion in owe you.
I have been able to communicate via RS232 and I2C very well. How ever I am confused how to pass data to and from the PSoC 3 & 5. I used paremeters for the RS232 communications. I not sure how to pass data from the analog section to the PC. Any snippets of code would be very helpful.
Thanks
Philip
Show LessHi, I have a new project developed in PSoC3, I need to establish Wi-Fi communication. The Ad-Hoc is ready but in EBK shows displayed message "RF Band select". I'm using this material:
Hardware
. Cypress, CY8CKIT-030 PSoC3
. RedPineSignals, RS-CY8C001-220X
Firmware
. LIB_TestPSoC3_UART.cywrk
Documentation
. RS-CY8C001-220X_EBK_User_Guide.pdf
Regards
BE Ezequiel Rivas
Show Less