PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Hi, when i used for the first time a cy8ckit-001, i could see selftest.hex ran in kit just with power connection, but, since i started to use the miniprog, i can't more to ran again the selftest.hex file or any other program with sucess without the miniprog plugged. If i unplug the miniprog, the program stop the function, and when i pressing the reset button, are displayed black squares in first line. Someone Knows in what cam i wrong?
Show LessWhen I enable differential mode on the PSoC 3 DelSigma ADC I get the following warning on buid:
Info: apr.M0002: Analog signal "\ADC_DelSig_1:Net_194\" is connected to one terminal only. (App=cydsfit)
I just have the ADC on the schematic with 2 analog pins feeding the input terminals. All the settings are at the default except the input range.
Is this warning safe to ignore or do I have larger problems?
Show LessHi all
Please help me how to make simple method TRNG (true random generator) from analog internal component for Psoc1 (CY8C29466)
Many thanks Kamil
Show Less Hi!
So, I have this project to do ''General analogue data acquisition and sending through SPI to PC on PSoC'', but I have no idea how to do it. I think it's PSOC 3.
My PSoC should be able to acquire any sort of analogue signal from any port on UNI-DS3 developement board, transfer it to digital, and then send it to PC through SPI.
I'm new to all of this, and I'm supposed to work in PSoC Designer 5.4, but don't know how to.
So I'm asking if someone is willing to help me, and teach me how to do it, or at least tell me what modules should I use, then I will study them on my own.
Help is urgently needed, since I have to be done with this in 3 weeks.
Regards Ivan.
I am attempting to complete a PSoC1 project involving using a 555timer circuit as a capacitance meter. Essentially the resistor/capacitor network in the circuit directly relates to the 555timer output in that t = 1.1RC. I am fine with the circuit design, my problem is in writing the main.c file for it. I need to be able to read in the 555 output, have PSoC recognize the T value, and calculate for capacitance and display it to the LCD. Any help would be greatly appreciated.
Show LessThe FMEA acronym is short for Failure Mode and Effect Analysis. This is analysis methodology used to detect the failure and take the appropriate action to avoid the malfunctioning of the device or system.
Hi everyone,
I recently updated PSoC Creator to V3.0, and I have a PSOC5 project i'm working on. The project worked just fine with the V2.2, and now I have this error when i'm try to compile it :
ADD: sdb.M0059: error: Error in component: cy_boot. The cy_boot_v3_40 component (cy_boot) is an Obsolete component. It is no longer recommended for use and should be replaced with a production version of the component (or an alternative implementation).
Error: cdf.M0005: CyDsFit aborted due to errors, please address all errors and rerun CyDsFit. (App=cydsfit)
Does anyone have an idea of what I can do to fix it?
Thank you
Nicolas
Show LessSo I modified the AN2283 FrequencyProject code provided on the Cypress Website (http://www.cypress.com/?rID=2671) so that it can read frequencies from a microphone. So what I really want to do is filter a siren from other noises and the siren fluctuates in the pattern of 1.5kHz to 2.0kHz to 1.5kHz. Would I have to use a while loop? I am not to familiar with C.
Here is a snip of the modified code and the project is also attached:
LCD_Position(0,0);
if (fFreqValue >= 1.4 && fFreqValue <= 1.6) {
if (fFreqValue >= 1.8 && fFreqValue <= 2.2) {
if (fFreqValue >= 1.4 && fFreqValue <= 1.6) {
LCD_PrCString("Siren Detected!");
}
}
}
else {
LCD_PrCString("Scanning... ");
}
Show Lessi am trying to use capsense slide to increase or decrease some values. My problem is i couldn't accurately choose the value by rubbing my figure on the capsense slide of CY8CKIT-001 demo kit. For example when i try to increase the value to 7, after increasing the value when i take my fingure out of the capsense slide, the value is changed to eigther 6 or 8 or some near by value. Can any body suggest which parameter of the capsense that i should change to get the consistant values.
kavin
Show Less