PSoC™ 5, 3 & 1 Forum Discussions
Hi Everyone,
I did not find the place to post my RF chip related question in forum so i am posting here.
I have choosed "CYRF69103" Chip for my application it has RF transceiver (upto 100m).
my questions are
1.How to i can program this controller?
2.when checked for reference design board , the product is no longer active. so how do i can start with this MCU?
thanks,
Ashok r
Show LessI have 2 questions?
Is the Suite USB 3.4.7 the latest version?
Which is a USB driver for Windows 7? (There are only w2k(for 2000), wlh(for Vista) and wxp (for XP).)
Regards
Qingshan
Show LessIs it possible to define an external command to be called each time I build my project? You see, I want to compile in values from my revision control system. We use TortoiseSVN, and there is a program called SubWCRev to use, http://tortoisesvn.net/docs/release/TortoiseSVN_en/tsvn-subwcrev-example.html
I also thought about solving this manually by always building my project from command line, by creating a build script. Is then the Cypress command line program cyprjmgr.exe the way to go? Actually, since I am a programmer, I prefer using command line anyway, so is it possible (in an easy way) to do building, programming and debugging from command line?
Show LessHello I made a code that use addition, subtraction and multiplication Here is the code
PART 1:
if (((atoi(anio)-1) % 4) == 0){
unix_Time =(atoi(anio)+30)*365+1+11;
}
else
unix_Time =((atoi(anio)+30)*365)+11;
PART 2:
case 4:
unix_Time +=120;
break;
PART 3:
unix_Time += atoi(dia)-1;
unix_Time is a long variable to save te sum of the operation but, the operation in part 3 the result is wrong because don´t make the rest of one. I have tried using the next code:
unixunix_Time += atoi(dia);
unix_Time --;
but it does not work, I have the same ressult. sombody help me ?
I have the CY3214-PSoC-EvalUSB development board and I've been making the Capsense example (5.1 - My First Code Example) as outlined in the user guide that came with the dev board.
I have been able to build and generate the project fine and even supposedly program the firmware onto the chip but when I power the dev board and try to press on the capactive pads/slider, nothing happens.
I then programmed the capsense example hex file that came bundled with the dev board CD and that actually worked but when I try to program my version of the example (which should be the exact same as what was bundled with the board), that's when things don't work. Am I just not creating the hex file properly?
The target chip is the CY8C24894-24LTXI and I'm using PSoC Designer 5.1
I've double checked the module parameters and the match what is specified in the user guide
I've copied the contents from the provided main.c file into my main file (as specified in the guide)
I've even cleaned and rebuilt the project hoping it would do something. It didn't.
The power jumper on the dev board is set to Vbus, which is where it should be
The Dev Board page is here: http://www.cypress.com/?rID=37815
The user guide is also in that page provided above.
Thanks for you help!
Show LessI used CY8C24533,CY8C27643 and CY8C29666, but only CY8C29666 save data to the E2PROM, if the address is wrong, the program area will be destroyed, such as digital controls are not displayed, the program can not run. Many similar situations happen, I need to address one by one to try, such as
save six bytes of data should be: E2PROM_E2Read (0, SAVE, 6);
but I need wirte :
E2PROM_E2Read (1, & SAVE [0], 1);
E2PROM_E2Read (7, & SAVE [1], 1);
E2PROM_E2Read (12, & SAVE [2], 1);
E2PROM_E2Read (18, & SAVE [3], 1);
E2PROM_E2Read (28, & SAVE [4], 1);
E2PROM_E2Read (58, & SAVE [5], 1);
who can help me???
Show LessHello everyone. I'm a newbie with PSoC, and I have a simple question (but with a hard solution, I think).
I'm using PSoC 3 in my little project. I'm sending data from the SRAM (a variable in the code), through USB to PC. I can see the data with Cypress Suite USB, and I check it's correct with the LCD. Now, the problem is that I need to see the data like in an oscilloscope (it can be any signal: sine, triangle, etc.). I just need to plot the data that I can read with "Cypress Suite USB". I'm using bulk transfer, but I could change it in the case it's necessary.
So, my question is: Is there an easy way for this?? I think the main problem is the communication, the way I get the data. The other part is to plot the data, it should be almost real time (no more than a second delay). I suposse I should make a program, but it could be very hard and long (I have never program a GUI, just with Matlab). I thought about Matlab, it could be very interesting (mainly for the plotting), but I have been reading about this and I think it's not possible to read data directly from an USB.
Thanks for the help 🙂
Show Lesshow much is the flexibility of psoc about implenting with UDBs
is there any way to have more than 192 UDB in psoc5lp
i have an project in verilog and when i build it with psoc creator i have this errors?
Resource limit: Maximum number of UDB Macrocells exceeded (max=192, needed=780).
Resource limit: Maximum number of UDB Unique Pterms exceeded (max=384, needed=2484).
my project is here
Show LessHi every one !
Please, can someone explain me how I shoud read Table 2. PSoC 3 8051 SFR Map at PSoC® 3 – 8051 Code and Memory Optimization - AN60630 ?
My be is a silly question by I do not understand what does mean the header over each colum. I do not Know if we are talking about Bytes o bits.
I undestand that ther are 128 byte in that block.
But, I can't undersatand wich is the start address of , let say, SFRPRT1DR, SFRPRT1PS, DPX0 and DPX1, for example.
Thank you very much for any help