PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Hi Every One !
I would need some help regarding noise generated for the Delta sigma in single end configuration.
As you can see in the schematic as result of array scanning I am geting pulses which votage depend of the pressure applied to every cell in the array. My Vdda is 3.3 v . The issue is that with no pulse, ( checked with osciloscope) there is noise that you can watch in the graphic display picture.
The only way to avoid that is using a PGA before the Delta sigma..
I cannot undestan that. !!!!
And even using a PGA, I need to filter trough code , like high pass filter values above 0x80, wich represent almost a half of the ADC range.
I woul appreciate very much any help.
Show LessHello Everyone,
Could you help me with my ADC, I cannot get it Right I want to use ADC for input range of (+/- 1.25) in a differential input range with a refrenve of vdda/4 = 1.25. could you tell me what is the voltage range and the corresponding digital value in decimal?
Thanks.
maxdamage.
Show LessCan anyone tell me what the problem I have with CY8CKIT-050 to measure the voltage of a resistance of 10 k to 100 uA idac is not true and then varies the channels are 5 v without having connected to the resistor. How do I can find the true voltage?
Show LessWhere do I get information on how to send data psoc 5 for graph to plot select program?
Hi,
I measured that the time for execution of the EEPROM_Write function is ca. 15 ms, which is far away from the typical value of 2 ms specified as "Single row erase/write cycle time". Is that possible or does this function have so much overhead time because it is doing a single row erase and write ?
BTW, I used the CySetTemp() function to compensate for temperature influence.
Thanks
Show LessHallo,
I want to design a project, where a reference is brought out on P0[0] with VDAC buffered by Opamp.
At the same time I want to measure the P0[0] with ADC_DelSig over AGL[4].
Please look at the attached project for full understanding.
The project works fine for Analog Mux but with the Analog HW Mux I get the following Error Message:
"Signal "\Opamp_1:Net_29\" is expected to connect to only one GPIO analog pin but instead it connects to "\Opamp_1:ABuf\". Please fix the connection."
(Please do not care about ADC_DelSig sampling or AMux switching, this is done later.
Only concentrate on the routing problem!)
regards Willi
Show LessHi. I am playing with PSoC3 USB bulk data transfer using CyConsole. all is working fine.
I can now manipulate the firmware per my application. However, I will need the PC (software) side.
Is there a CyConsole code/project for the PC - in VB.net or VC#.net? Thanks.
Show LessHi. how do I change an IO pin from an output to an input pin (or vise versa) in code?
The datasheet for IO has one API called CyPins_SetPin() but its usage (API) wasn't described. Is this what I need?
The code generated for the project (Pin_1.c) does not even contain this routine (?)
This API is for use with PSoc3 and PSoC5LP which are both of the devices that I am using.
Please advise. Thank you.
Show Less¿Cómo puedo medir la diferencia de potencial en un período de tiempo utilizando adc y usb psoc 5?
Hello everyone,
I'm trying to make my own PSoC 5lp board currently. I'm wondering how can I draw CY8C58LP chip in schematic and generate pcb as well. Thanks a lot!
Show Less