PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Hello,
I can't find examples of this in C or with the Built in modules. How would I make a task scheduler so that I can read my ADC switch Channels and read again.. and so on.
Thanks, Examples are usually the best
Show Lessi need one basic Band pass filter design code. .. i am not able develop the code for BPF . i already checked all vedio which is not explaning everything about Filter design coding ...
Show LessNeed to be pointed in the right direction for using the USB UART on Windows 8, which has strict digital signature enforcement.
Getting a prototype ready for a trade show I found that a Windows 8.1 tablet would not accept the unsigned setup .inf file so I came to the Cypress site and ran an installer that put drivers in Program Files (x86). It appears that the configuration of the part in Creator must be changed to be compatible with the .inf file. If this is true, not sure which strings to change. Also noticed there was no reference to usbser.sys in the file. Do I need to use some other driver?
Also, would like to get a digital signature for our product and modify the .inf file to use our corporate USB PID and VID. Should I open a case for this?
Show LessHi,
I would like to ask you for help in programming SPI where I completely lost. I send what I have done. Thank you so much for your advice. I would like to ask you a very, if you give me a program finished typing. Thank you
Show LessI believe I am having troubles in setting the right Frequencies / global values for my Project. I am uprgrading to a Cypress - CY8C27443-24SXI and the Previous Chip's cpu clock ranged from 4.2MHz - 6.0MHz.
I am sending hi or low signals from my CY8C27443-24SXI to an analog multiplexer which I believe averaged to be roughly 2.5kHz
Any help with these would be appreciated, please let me know if anyone would like more info.
Thanks
Show LessHello, I am currently using ADCIN and I'm wondering if theres a way to "pause" the ADC for a certain time. Right now I'm setting pins that read from an external mux which sends back to my ADC in two different Channels. I have narrowed it down to most likely reading data too fast.
AMUX4_1_InputSelect(AMUX4_1_PORT0_3);
Set_Port0_1(0);
Set_Port2_7(0);
Read_ADC();
Let me know if you need more info
Show Lesshello every one,
I want to know exactly what i have to put like a parameter in the Instrumentation amplifier to get a signal in the output .
i specify that i use a mesure of biceps muscle .
so please help me gays
Show LessI'm trying to update the software for a firmware chipset, and I'm having trouble understanding how variables are passed between C and assembly. When I try to compile, I get these errors:
https://gist.github.com/anonymous/d79f8f9734865a3ec1fe
These variables are defined in global.h here:
https://gist.github.com/anonymous/d81de7895838eaa41361
Also, lib/timer8_1int.asm is pretty short, so here it is:
https://gist.github.com/anonymous/848875129e7cf16e110f
Thank you for your time.
I'm using PSoC Designer 5.4 to write and compile this code, if that helps anyone.
My os is win7(64bit)
PSoCCreatorSetup_3.1_sp2_3-26-15(I download it from here)
when i creat a new project there is no device.h in my header files
what can i do?
Show LessI'm trying to update the software for a firmware chipset, and I'm having trouble understanding how variables are passed between C and assembly. When I try to compile, I get these errors:
https://gist.github.com/anonymous/d79f8f9734865a3ec1fe
These variables are defined in global.h here:
https://gist.github.com/anonymous/d81de7895838eaa41361
Also, lib/timer8_1int.asm is pretty short, so here it is:
https://gist.github.com/anonymous/848875129e7cf16e110f
Thank you for your time.
I'm using PSoC Designer 5.4 to write and compile this code, if that helps anyone.