PSoC™ 5, 3 & 1 Forum Discussions
PSoC™ 5, 3 & 1
Hello, I know that PSoC 3 has no SD card module so I want to know if there is any other way to store data on an SD card e.g. using I2C ...
Show More
Hello,
I know that PSoC 3 has no SD card module so I want to know if there is any other way to store data on an SD card e.g. using I2C or sth.
I am new to PSoC and a not-so-experienced programmer, so please respond accordingly.
Thanks. Show Less
I know that PSoC 3 has no SD card module so I want to know if there is any other way to store data on an SD card e.g. using I2C or sth.
I am new to PSoC and a not-so-experienced programmer, so please respond accordingly.
Thanks. Show Less
PSoC™ 5, 3 & 1
hi sorry for this complete newbie question i don't even know, if this is the right forum to post this question ! we have to t...
Show More
hi
sorry for this complete newbie question
i don't even know, if this is the right forum to post this question !
we have to talk to a "CY3240-I2USB" bridge via C++,
(VisualStudio Pro 6.0)
but have only found an activeX control
and an example that works only for VS .NET 2005 or higher
isn't there any library (= simple dll, lib or header files)
to get access to the CY3240-I2USB ?
can the "SuiteUSB" be used for this device ?
http://www.cypress.com/?rID=34870
any help is appreciated ! Show Less
sorry for this complete newbie question
i don't even know, if this is the right forum to post this question !
we have to talk to a "CY3240-I2USB" bridge via C++,
(VisualStudio Pro 6.0)
but have only found an activeX control
and an example that works only for VS .NET 2005 or higher
isn't there any library (= simple dll, lib or header files)
to get access to the CY3240-I2USB ?
can the "SuiteUSB" be used for this device ?
http://www.cypress.com/?rID=34870
any help is appreciated ! Show Less
PSoC™ 5, 3 & 1
Just started to use PSoC Designer 5 SP 6. When I compile and click on errors listed in the output from Build screen, Designer no longer jumps ...
Show More
Just started to use PSoC Designer 5 SP 6. When I compile and click on errors listed in the output from Build screen, Designer no longer jumps to the file and line of code containing the error.
using WIN XP Pro Show Less
using WIN XP Pro Show Less
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
I talked to the local rep yesterday and was told that PSoC Creator will include a full C Compiler for the PSoC5. Does this mean that GCC will ...
Show More
I talked to the local rep yesterday and was told that PSoC Creator will include a full C Compiler for the PSoC5. Does this mean that GCC will be used?
Will the SWD debug support ITM channels as defined in ARM CMSIS documentation?
Are there any kits currently available with the PSoC5?
Rep indicated that it will probably be 2Q next year before wilicon is available to sample. Is this true for eval kits/modules as well?
When will PSoC Creator component libraries be updated to provide master I2C?
Is it true that Verilog can be used for components? Show Less
Will the SWD debug support ITM channels as defined in ARM CMSIS documentation?
Are there any kits currently available with the PSoC5?
Rep indicated that it will probably be 2Q next year before wilicon is available to sample. Is this true for eval kits/modules as well?
When will PSoC Creator component libraries be updated to provide master I2C?
Is it true that Verilog can be used for components? Show Less
PSoC™ 5, 3 & 1
Hello *, I am new here and new to PSoC from Cypress. My enterprise "electronica@tdnet UG" and all of corporated enterprises usin...
Show More
Hello *,
I am new here and new to PSoC from Cypress.
My enterprise "electronica@tdnet UG" and all of corporated enterprises using exclusively the Linux Operating System and now I like to know, which tools I need to code under Linux without the need to buy usesless proprieatary stuff from Redmond.
Note: I do NOT use KDE/GNOME or other Desktop Environment. No, no Eclipse or such. Only plain TEXTEDITOR and Debuger and Compiler (I programmed my first 8039 in 1982 by feet using a switchboard for the addresses and data and a button to burn adress after adress)
Thanks in Advance
Michelle Konzack
Owner and Chefdeveloper
Tamay Dogan Network Show Less
I am new here and new to PSoC from Cypress.
My enterprise "electronica@tdnet UG" and all of corporated enterprises using exclusively the Linux Operating System and now I like to know, which tools I need to code under Linux without the need to buy usesless proprieatary stuff from Redmond.
Note: I do NOT use KDE/GNOME or other Desktop Environment. No, no Eclipse or such. Only plain TEXTEDITOR and Debuger and Compiler (I programmed my first 8039 in 1982 by feet using a switchboard for the addresses and data and a button to burn adress after adress)
Thanks in Advance
Michelle Konzack
Owner and Chefdeveloper
Tamay Dogan Network Show Less
PSoC™ 5, 3 & 1
Hello, I'm trying to implement the Application note 2207 to build a milliohmeter. It's my first try on PSOC device and I face a problem...
Show More
Hello,
I'm trying to implement the Application note 2207 to build a milliohmeter. It's my first try on PSOC device and I face a problem.
I implement the power supply provided in the AN but when I load the circuit with the PSOC device (CY8C27) the voltage falls to 2.8V instead of 5.5V.
I use the LP2950 voltage regulator that is designed up to 100 mA (the AN indicate 55mA consumption), so it seems OK.
Do you have any idea to fix my problem? Do you have complete schematics in Orcad format of the AN2207 ?
Best regards Show Less
I'm trying to implement the Application note 2207 to build a milliohmeter. It's my first try on PSOC device and I face a problem.
I implement the power supply provided in the AN but when I load the circuit with the PSOC device (CY8C27) the voltage falls to 2.8V instead of 5.5V.
I use the LP2950 voltage regulator that is designed up to 100 mA (the AN indicate 55mA consumption), so it seems OK.
Do you have any idea to fix my problem? Do you have complete schematics in Orcad format of the AN2207 ?
Best regards Show Less
PSoC™ 5, 3 & 1
Problem: When System clock is selected as P1[4] in PD5.0 SP5, PSoC does not work. Work Around: Following is the work around: S...
Show More
Problem:
When System clock is selected as P1[4] in PD5.0 SP5, PSoC does not work.
Work Around:
Following is the work around:
Select SysClock Source as Internal.
Set drive mode for P1.4 as High-Z.
Now you have two options (you can use either of them):
1. Write instruction OSC_CR2 = 0x06; in main.c. It will shift to System Clock to External Clock from IMO
2. Open boot.tpl file and add following lines in boot.tpl below line "lcall LoadConfigInit".
M8C_SetBank1
mov reg[OSC_CR2], 6
M8C_SetBank0
Now your code in boot.tpl should like following near above line:
lcall LoadConfigInit
M8C_SetBank1
mov reg[OSC_CR2], 6
M8C_SetBank0
It will shift to System Clock to External Clock from IMO
But make sure that you keep SysClock Source as Internal and drive mode for P1.4 as High-Z in device editor.
This issue will be fixed in PD5.0 SP6. Show Less
When System clock is selected as P1[4] in PD5.0 SP5, PSoC does not work.
Work Around:
Following is the work around:
Select SysClock Source as Internal.
Set drive mode for P1.4 as High-Z.
Now you have two options (you can use either of them):
1. Write instruction OSC_CR2 = 0x06; in main.c. It will shift to System Clock to External Clock from IMO
2. Open boot.tpl file and add following lines in boot.tpl below line "lcall LoadConfigInit".
M8C_SetBank1
mov reg[OSC_CR2], 6
M8C_SetBank0
Now your code in boot.tpl should like following near above line:
lcall LoadConfigInit
M8C_SetBank1
mov reg[OSC_CR2], 6
M8C_SetBank0
It will shift to System Clock to External Clock from IMO
But make sure that you keep SysClock Source as Internal and drive mode for P1.4 as High-Z in device editor.
This issue will be fixed in PD5.0 SP6. Show Less
PSoC™ 5, 3 & 1
When you try to open PSoC Designer, you get the error message "To view this file you must download Adobe SVG viewer". This problem can ...
Show More
When you try to open PSoC Designer, you get the error message "To view this file you must download Adobe SVG viewer".
This problem can be due to IT policies on your machine. To fix this issue, registry need to be edited. To modify the key:
1. Click Start, click Run, type Regedit in the "Open" text box, and then click OK.
2. Locate the following registry key.
HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Internet Explorer \Main\FeatureControl \ FEATURE_LOCALMACHINE_LOCKDOWN
3. Crete a backup of this registry entry. To create backup:
4. On the Edit menu, point to New, and then click DWORD Value.
5. In the DWORD Value box, type psocdesigner.exe, and then press ENTER.
6. Double-click the psocdesigner.exe registry entry that you created in step 4.
7. In the Value data box, type 0, and then click OK.
8. Repeat steps 4-7 to add CMX.exe.
9. Exit Registry Editor. Show Less
This problem can be due to IT policies on your machine. To fix this issue, registry need to be edited. To modify the key:
1. Click Start, click Run, type Regedit in the "Open" text box, and then click OK.
2. Locate the following registry key.
HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Internet Explorer \Main\FeatureControl \ FEATURE_LOCALMACHINE_LOCKDOWN
3. Crete a backup of this registry entry. To create backup:
- File > Export
Save the .reg file
Later if you need to restore old settings, File > Import the same .reg file
4. On the Edit menu, point to New, and then click DWORD Value.
5. In the DWORD Value box, type psocdesigner.exe, and then press ENTER.
6. Double-click the psocdesigner.exe registry entry that you created in step 4.
7. In the Value data box, type 0, and then click OK.
8. Repeat steps 4-7 to add CMX.exe.
9. Exit Registry Editor. Show Less
PSoC™ 5, 3 & 1
Hi All, i am new to this forum, i'm working on cypress controller for the past 2 months. Doubts: 1. In my firmware, I h...
Show More
Hi All,
i am new to this forum, i'm working on cypress controller for the past 2 months.
Doubts:
1. In my firmware, I have set the Enpoint(6) buffer size as 512. But, in Get Transfer Size API call (for respective Endpoints - 6) is returning size as 4096.
why it is happenning ? if my endpoint size is 512 why it is returning 4096.
Transfer Size should be same as the Endpoint Buffer Size. if not, tell me for what purpose trasnfer size is using...
Please clarify the same
2. By Default, Cypress speec is high speed. Can you tell me Cypress API which will set the speed?
3.i need the reponse time for XferData Function, it is taking more than 16ms for getting data from board (in HIGH Speed) ?
Please Clarify my doubt as soon as possible.
Thanks
Ram Show Less
i am new to this forum, i'm working on cypress controller for the past 2 months.
Doubts:
1. In my firmware, I have set the Enpoint(6) buffer size as 512. But, in Get Transfer Size API call (for respective Endpoints - 6) is returning size as 4096.
why it is happenning ? if my endpoint size is 512 why it is returning 4096.
Transfer Size should be same as the Endpoint Buffer Size. if not, tell me for what purpose trasnfer size is using...
Please clarify the same
2. By Default, Cypress speec is high speed. Can you tell me Cypress API which will set the speed?
3.i need the reponse time for XferData Function, it is taking more than 16ms for getting data from board (in HIGH Speed) ?
Please Clarify my doubt as soon as possible.
Thanks
Ram Show Less