PSoC™ 5, 3 & 1 Forum Discussions
Hi,
I my application I am using a piezo element as a microphone.
I need to amlify and process it but I have 2 problems:
1. How to make a charge mode amplifier using an internal Op-amp (single supply ).
2. How to interface the mic with the chip.
Please help...
Anna
Show LessI am trying to change the duty cycle of signal. if I set higher period for PWM component, i can acheive the duty cycle whereas I am not geeting the exact frequency.
I am using Timer(tc) to input the PWM.
How can I acheive the duty as well as correct frequency?
Show LessHi guys,
I am confised about CY8CMBR3116 programmer. Can I program it with CY3217 or CY3210 mini programmer.
What is your suggest to program CY8CMBR3116.
Second question:
I know CY3210 mini programmer is old version. (CY3217 is new). But I want to use CY3210 to program CY8C21x34 (CY8C21434-24LTXI). It is possible?
Thanks
Show LessI am trying to change the duty cycle of signal. if I set higher period for PWM component, i can acheive the duty cycle whereas I am not getting the exact frequency.
I am using Timer(tc) to input the PWM.
How can I acheive the duty as well as correct frequency?
Show LessHi
I have CY8CKIT PSoC 5LP KIT and I want to measure time between 6 signals that coming on 6 different pins.
First signal is TR. When TR happened (rising edge) 5 time counters start.
When MP1 happened (rising edge) first counter stop.
When MP2 happened (rising edge) counter 2 stop.
All same to MP5.
After 100 ms send 5 time values ( number in ms) to COM Port (RS232).
If I have 2 TR before MP that counter send message AAAAAAAA.
If MP don't happened 100 ms after TR that counter send message CCCCCCCC.
I am new to PSoC and don't have C code experience.
Can somebody help me with this?
Thanks
Val
Show LessDear all:
I am trying to communicate with analog Devices part AD7793 using SPI with a PSOC5.
I have CY8CKIT-050 and the AD7793 Evalutaion KIT (I need more ADC channels so I need AD7793 for these extra channels). I wired the signals mosi, miso, cs , clk and GND beween both EVK.
AD support this devices with a generic diver that can be download from http://wiki.analog.com/resources/tools-software/uc-drivers/renesas/ad7793
I also attach the project on PSOC with a vey simple main.c. I Just want to check the AD7793 is there using function AD7793_init();.
I am not able to talk with AD7793. Can anyone have a look to the SPI communication function and check if there is any wrong.?
Thanks in advance,
Joaquin.
Show Less