PSoC™ 5, 3 & 1 Forum Discussions
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
I used the ADC example with the pot. It worked great. When I added a mux and the 16 input channels the ADC complained about: ERROR: C:\...
Show More
I used the ADC example with the pot. It worked great. When I added a mux and the 16 input channels the ADC complained about:
ERROR: C:\DESIGN01\DESIGN01.CYDSN\GENERATED_SOURCE\PSOC3\ADC_DELSIG_2.C:70: 'CyIntSetPriority': requires ANSI-style prototype Show Less
ERROR: C:\DESIGN01\DESIGN01.CYDSN\GENERATED_SOURCE\PSOC3\ADC_DELSIG_2.C:70: 'CyIntSetPriority': requires ANSI-style prototype Show Less
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
I am looking in to implementing a hw-controlled gain stage so either a 2 fix-gain PGAs and a-mux or a hw-controlled gain PGA. It does not seem...
Show More
I am looking in to implementing a hw-controlled gain stage so either a 2 fix-gain PGAs and a-mux or a hw-controlled gain PGA. It does not seem possible with current Psoc?arch.
Show Less
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
hi sorry for this complete newbie question i don't even know, if this is the right forum to post this question ! we have to t...
Show More
hi
sorry for this complete newbie question
i don't even know, if this is the right forum to post this question !
we have to talk to a "CY3240-I2USB" bridge via C++,
(VisualStudio Pro 6.0)
but have only found an activeX control
and an example that works only for VS .NET 2005 or higher
isn't there any library (= simple dll, lib or header files)
to get access to the CY3240-I2USB ?
can the "SuiteUSB" be used for this device ?
http://www.cypress.com/?rID=34870
any help is appreciated ! Show Less
sorry for this complete newbie question
i don't even know, if this is the right forum to post this question !
we have to talk to a "CY3240-I2USB" bridge via C++,
(VisualStudio Pro 6.0)
but have only found an activeX control
and an example that works only for VS .NET 2005 or higher
isn't there any library (= simple dll, lib or header files)
to get access to the CY3240-I2USB ?
can the "SuiteUSB" be used for this device ?
http://www.cypress.com/?rID=34870
any help is appreciated ! Show Less
PSoC™ 5, 3 & 1
PSoC™ 5, 3 & 1
When placing I2CHW as slave in 28445 I see the parameter Auto_Addr_Check, which I don't recall seeing before. It is not mentioned in the modul...
Show More
When placing I2CHW as slave in 28445 I see the parameter Auto_Addr_Check, which I don't recall seeing before. It is not mentioned in the module's datasheet. What is this for?
Show Less
PSoC™ 5, 3 & 1
Just started to use PSoC Designer 5 SP 6. When I compile and click on errors listed in the output from Build screen, Designer no longer jumps ...
Show More
Just started to use PSoC Designer 5 SP 6. When I compile and click on errors listed in the output from Build screen, Designer no longer jumps to the file and line of code containing the error.
using WIN XP Pro Show Less
using WIN XP Pro Show Less