PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
Where can I download HighResDacs libraries?
Hii everyone,
I am new to Psoc I am taking analog signal and giving to ADC and then to Filter through DMA and then passing to PC through USBUART.
My concern is when I use less sampling rate in ADC and transfer the signal through USBUART I could plot in MATLAB in realtime and changes are also reflecting simultaneously. But when I use high sampling rate in ADC and when I transfer through USBUART I could able to plot but there is lot of delay. If I change the input It is reflecting after long time.
I am using 8bit ADC and I am transferring though USBUART by using USBUART_PutData(&Output,1); and in matlab I am reading one byte at a time and plottitng the graph.
Please help me regarding this.
Thank you
Hem k
Show LessChip on board : CY8C3866AXI-040ES2 0913A 04 613205
Little i knew about backward incompactibility before purchasing so many of these kits. After Quick research, majority of the pages suggested either get it exchanged (Exchange period is now over) or use old version of creator.
If any one have gone through this earlier, it will save me a lot of time and effort. Is it possible program these kits using different version of PSoC Programmer and device drivers but generate the hex from latest version of creator.
Thank you
Show LessHi All,
I am looking for a way through which I can shift my signal by 90 degrees. I want to avoid using flip flops.
Looking forward to your suggestions.
Regards
Awais
Show LessHi,
Is there any pins on the CY8CKIT-059 where I can output a clock?
I have tried to use a GPIO to output a 1.5 MHz clock, but it doesn't look very nice on a oscilloscope. Is there a recommended way of doing this?
Show LessHello Everyone,
I am using PSOC 3 family right now am working on UART communication where am trying to use only one UART component then it should able to work on different baud rates based on the input (actually the input signal is available on various baud rates )so it has to detect the input baud rate automatically and then able to function accordingly based on the baud rate
so can anybody suggest me how to configure different baud rates for same UART component
Note :Actually if i set individual baud rate (using clocks it is working correctly) but i would like to create the functions to detect and respond accordingly for various baud rate inputs
ANy help or ideas or suggestion would be greatly apppreciated
thank you
prabhu
Show LessHI,
i am following this website
here i am trying to add a new rtos task and want to give delay but in that project i am unable to modify delay.
since i am new to psoc can you tell me how to set pin for GPIO and set delay by using programming not by vydwr file where you just change pin button by GUI. That i do not want. I want the layer where pin no and delay can change.
Thank you
so please help me out
Show LessHelp Regarding,
CY8C5888LTI-LP097 QFN68
I am trying to port FREE RTOS in CY8CKIT-059 for that i am following link
But i am unable to build error is coming while loading. I have attached the details in picture please help me i am new to this microcontroller and FREE RTOS.
Thank you
Show LessHi all
I need to design the notch filter for removing 50hz noise. But i dont know how to design my own component. Give some useful reference. In my previous post odissey gave me the link of notch filter but my problem is i dont know how to design my own filter. I am new to in this field can any one help me.
Show Less