PSoC™ 5, 3 & 1

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
KevinE
PSoC™ 5, 3 & 1
I am working with CY8CKIT-059 and need help discerning the differences between my custom project and one of the projects provided under "Find code exa... Show More
jadkh
PSoC™ 5, 3 & 1
Hello Infineon community! I finally received my CY8CKIT-059 PSOC5LP. I am a total beginner working with it but I'm looking forward to doing my project... Show More
jadkh
PSoC™ 5, 3 & 1
Hello Infineon World!  I'm using PSoC 5LP (CY8KIT-59) and I'm reading the data of a 3 axial accelerometer using the 3 ADCs. I want to send the 3 axis ... Show More
JulianLBTK
PSoC™ 5, 3 & 1
Hi everyone... I'm working with the DS18B20 temperature sensor and I'm using One-Wire Protocol,  the project is working well but I have a question: Wh... Show More
Yash_r
PSoC™ 5, 3 & 1
Hello @MotooTanaka san, I have been trying to get this example as a base to implement a simple HMI menu system using PSOC 5LP and 4x4 keypad and LCD: https://community.cypress.com/t5/Code-Examples/4x4-Matrix-Keypad-Sample/m-p/96977#M370... Show More
nigelsmith
PSoC™ 5, 3 & 1
I'm trying to automate the programming of a CY8C3445AXI-104 device using the ppcli application, the problem I have is that I cannot find the ppcli com... Show More
Rolf_Nooteboom
PSoC™ 5, 3 & 1
For the ones interested, I created a Visual Studio Code setup for PSoC5.   The setup makes use of PSoC Creator which is needed for the (one time) conf... Show More
ArthurLuo
PSoC™ 5, 3 & 1

 Need CY8CTMA768AS-33 datasheet, Pinout, Programing guide. THKS.

RiMo_301056
PSoC™ 5, 3 & 1
Hi all, I got stuck trying to get sleep / wakeup running on a PSoC3. It seems that the device goes to sleep correctly, as I do this: sleep components... Show More
Dimaty
PSoC™ 5, 3 & 1
Hi, I have a cy8ckit-059 and I would like to power it using a 3.7V battery previously used in a drone. I would like to have a button that turns the sy... Show More
Board Information

PSoC™ 5, 3 & 1

The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
Top liked authors