PSoC™ 5, 3 & 1 Forum Discussions
text.format{('custom.tabs.no.results')}
I've noticed, that row latch ending with 0xB6 locks flash controller for one, last byte upload, resulting in random wrong row programming. There is a need of additional instruction for rowSize + 1 row latch data loading ( generally it is dummy operation, as long as row latch is "pseudoclosed" after receiving rowSize bytes ). RM should be corrected.
Show Lessi AM TRYING TO REBUILD THE RTD EXAMPLE OF PSOC3_4 FOR PSOC5LP KIT BUT MY RTD READINGS ARE NOT PROPER DUE TO IDAC NOT SOURCING PROPER 1MA CURRENT.
i TRIED 1MA SOURCING IN DIFFERENT EXAMPLE OF IDAC8 OF 5LP . HERE IT WORKS FINE BUT IN RTD EXAMPLE IDAC JUST SOURCE 0.22microamps and not 1ma.
please help as this is weird situation
Show LessI just it tried and this project has problem calibration register and temperature register.
Hello, I'm using a Mems 25Mhz clock and a Mems 32.768Khz clock on the MHZXIN and KHZXIN respectfully. I need a little help setting up the clock tree in my project in PSOC Creator 4.1.
Here is my schematic:
Here is my clock settings:
If anyone can give me some help I would greatly appreciate it.
Thanks,
Joe
Show LessWhen I compile I get Errors indicating "No input in instance" on TopDesign sheet. There are no Errors on the sheet, and the CPU program fine
Show Lesshi
i am new in cypress..i bought a psoc1 board and a miniprog 3 programmer..i install psoc designer in windows 7 pc, when i compile i am getting an error like this
Starting MAKE...
creating project.mk
name translation failed on C:/Program\ Files\ (x86)/Cypress/PSOCDE~1/5.4/Common/CYPRES~1 - 3
name translation failed on C:\Program - 2
name translation failed on Files - 2
name translation failed on (x86)\Cypress\PSOCDE~1\5.4\Common\CYPRES~1\tools\include\CY8C28~1 - 3
lib/psocconfig.asm
!E lib/psocconfig.asm(19): file 'm8c.inc' not found in current directory or in include path(s)
!E lib/psocconfig.asm(56): no such mnemonic 'RAM_PROLOGUE'
!E lib/psocconfig.asm(62): no such mnemonic 'RAM_EPILOGUE'
!E lib/psocconfig.asm(86): no such mnemonic 'RAM_PROLOGUE'
!E lib/psocconfig.asm(89): no such mnemonic 'M8C_SetBank0'
!E lib/psocconfig.asm(104): no such mnemonic 'M8C_SetBank0'
!E lib/psocconfig.asm(107): no such mnemonic 'RAM_EPILOGUE'
!E lib/psocconfig.asm(129): no such mnemonic 'RAM_PROLOGUE'
!E lib/psocconfig.asm(142): no such mnemonic 'M8C_SetBank0'
!E lib/psocconfig.asm(143): no such mnemonic 'M8C_ClearWDT'
!E lib/psocconfig.asm(152): no such mnemonic 'M8C_SetBank1'
!E lib/psocconfig.asm(172): no such mnemonic 'RAM_EPILOGUE'
make: *** [lib/obj/psocconfig.o] Error 1
make: *** Deleting file `lib/obj/psocconfig.o'
PDProject3 - 14 error(s) 0 warning(s) 19:48:04
i done lot of searing to find a solution for this problem...i tried all solution which i got from different discussion forums, but i have no luck..please help me to solve this
Show LessHello fellow developers 🙂
Using the PSOC 5, when connecting the USB to a PC the "USB UNKNOWN" message pops up.
1. I've used several designs with a usbuart feature. while on a different board the USB is recognized, on my board it isn't.
2. since my USB traces go through a VPX connector to another board and only then to a USB connector, I bypassed my board by attaching the USB cable straight to the 22.1 ohm resistors on both + and - pins (connected GND as well) - result was the same. UNKNOWN DEVICE.
3. I even replaced the device on my board from a 2015 date code to a 2017 date code, thinking that could be the problem.
So far I'm quite desperate.
Since I'm sure in my schematic, I think there are 3 issues that could be the problem:
1. I'm missing some kind of first time assignments to the device?
2. The burning in is somehow not correct (it says "successful" so i doubt it's the problem. but occasionally i get an error on first burn-in and succeed only in the 2nd try)?
3. I have some peripheral issues with voltages/currents/reset/capacitors/traces?
Can anyone assist? Have an idea on what I should check?
Thank you!
Sheran
Show LessOn PSOC5LP P0[2] and P0[4] are dedicated to the connection of an bypass capacitor for ExtVrefL_1 and EXTVrefL_2 (internal Vref of each SAR ADC).
Alas when using the internal OPA of the PSOC5 these two pin are assigned to the non inverted input.
Using internal OPA and Vref bypass capacitor at the same time is the goal.
Is it possible to bypass the internal Vref by connecting it to another analog output and place a discrete capacitor to GND?
Any suggestion of an alternate connection point is welcome.
Does anybody know how to measure a temp using a 10K thermistor and a psoc 5 I tried using the sample code but it does not work with the psoc 5LP CY8C5888LT*-LP097' any help would you guys could give me would be awesome thanks for your time I attached my code
Show LessHi
I am building a analog project using CY8CKIT-050 PSoC® 5LP Development Kit.
- What is the specifications of the internal components e.g. what is the specs of the opamp in terms slew rate, gain bandwidth product, etc.
- Is there any document listing these details ??