PSoC™ 5, 3 & 1 Forum Discussions
I use PP_ComLib_Wrapper.dll in my project. I have created an object with that dll:
static PP_ComLib_WrapperClass pp = new PP_ComLib_WrapperClass();
and when i try to use the function USB2IIC_DataTransfer , i come up with this error: "I2C_PerformTransaction() is not implemented by this Programmer".
And also when i try to use the function USB2IIC_SendData , i get this one: "USB2IIC_SendData() not implemented for this programmer!"
How can i solve this error? What should i do? I use kitprog 3 "KitProg3 (Bridge/0C170AEE00162400)"
Show LessI'm trying to understand the USB setup. I have a board that has a USB connector connected to the DP and DM pins on the PSOC5. I copied the code from the USBFS example and it runs, but hangs when trying to check the configuration. That appears to be because the Windows 10 computer does not recognize the USB device. It shows up in device manager under "Universal Serial Bus controllers", as "Unknown USB device (Device Descriptor Request Failed)". I am not sure if this is a hardware or software issue. The various documents seem to indicate that I have to find and install a special Windows device driver for the USBFS. I followed the instructions to install it but when I selected the .inf file, I got a message that a compatible file was not found. (That was when trying to install the driver from the unknown USB device entry in device manager.)
In general, why should I need a special device driver? I want to produce a product that creates a com port for anyone who installs it into windows. Why won't the Ftdi drivers work? Is there any path to making them work?
But, from reading, I am not at all sure that this is a driver problem.
Help please.
Thanks Russ
Show LessHi,
I set up a CAN component with multiple mailboxes. How can set only certain mailboxes to acknowledge messages while other mailboxes shouldn’t. I would need this functionality because I place a PSOC in a CAN network, where it should only listen to the ongoing traffic. At a certain moment I bring another device in to talk to the PSOC. Here I need it to acknowledge messages.
How do set this up? Is it possible to select which mailboxes should acknowledge and which not?
I really hope so, as I don’t really like to config two CAN components to do so.
Best, rose
Show LessI am encountering several build errors when attempting to connect the program to the microcontroller in the IDE. The errors I'm receiving are as follows:
- "Build error: cannot find -lEZPSoC5"
- "Build error: cannot find -lemf32noslfn"
- "Build error: The command 'arm-none-eabi-gcc.exe' failed with exit code '1'."
I'm unsure how to resolve these errors and would appreciate any assistance you can provide. Could you please explain what these error messages mean and what steps I should take to address them? I am using the PSoC 4.4 IDE and a PSoC 5lp Microcontroller
Thank you for your help.
Show LessHello,
I am attempting to communicate to my CY8CKIT-030A on my Windows machines via the USB/UART bridge.
On 2/27/24, Windows was able to detect my board as a COM port and I could communicate to the device with no issue.
Returning to my project a couple weeks later and now the board does not come up in the list of available COM ports in Device Manager. Additionally, I tried it on my co-workers system, and that system encountered the same issue.
I installed the latest version of PSoC Creator on a brand new Lenovo ThinkStation and encountered the same issue.
I can see the DVKProg(3.4.1.20) listed in the USB controllers.
Any help getting this board operational again would be greatly appreciated.
Show LessNot finished here was a link to these HW examples the community did in Verilog
and Schematic Capture (item 1 in request) :
https://community.infineon.com/t5/PSoC-5-3-1/Broken-Important-Links/td-p/439716
I have these examples and could zip them all and upload. I think they should be added
as a specific item to this page :
Let me know who to send the file to....
Regards, Dana.
Show LessI am working on PsoC 5LP (CY8CKIT-050) (MASTER) and I am connecting a sensor (SLAVE) which is RS485 variant. I am using a convertor for converting from RS485 to RS232 so to connect on the RS232 port of the kit. In order for the sensor to get ON, I need to set Holding register 40001 as 1. Could someone please help me with the coding part?
Show LessHello everyone,
I'm experiencing difficulties installing the KitProg Programmer drivers on my system running Windows 11. Each time I attempt to install, Windows fails to find the appropriate drivers for the device, as illustrated in the attached screenshot. I've attempted the usual methods such as searching for updated drivers through Windows Update, but to no avail.
Could someone guide me on how to properly install the KitProg Programmer on a Windows 11 system, or provide a link to the specific drivers required? Your assistance would be greatly appreciated to resolve this situation.
Thank you!
Show Less
The question "Why my questions are not indexed in this forum?" suggests that the individual is experiencing an issue with their questions not being properly indexed or searchable within a specific online forum. This could imply that when they search for their own questions within the forum's search functionality, they are unable to find them.
The question indicates a desire for clarification or assistance in resolving this problem. It could be due to various reasons such as technical issues with the forum's indexing system, the questions not meeting certain criteria for indexing, or the questions being buried among other content due to low visibility. Additionally, it might prompt discussions on best practices for ensuring questions are properly indexed within online forums to maximize their visibility and accessibility to other users.
Show LessHi community,
I used to see all available code examples when clicking on the link Start->Find Code Example. Also all the project that are available for download.
Since a couple of days I only see the downloaded projects and no projects available for download. What am I missing ?
There is no update available for the Creator.
Thanks for any help.
Cheers
Stefan
Show Less