Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

Hello, I could say that I'm doing wrong when I measure a sine signal using a filter and I get some voltage spikes are we of that wave

16 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Can you please post your complete project, so that we all can have a look at all of your settings? To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.

   

 

   

Bob

0 Likes
lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

here this file

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I have no experiences with ADC configured as left align, Did you try using right align?

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Looks like your signal us unsigned values and the filter is treating the values as signed.

   

That gives a spike at the signed rollover.

   

Magnus

0 Likes
EvPa_264126
Level 7
Level 7
500 replies posted 250 replies posted 100 likes received

if you comment out the line 63 the voltage spikes disappear.
difficult to understand the work Filter_SetDalign () and Set Coherency ()
 

0 Likes
lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

I did considering the filter Datasheet

   

0 Likes
lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

solve the problem, change input range Vss to vdd

   

thank you for your help

0 Likes
EvPa_264126
Level 7
Level 7
500 replies posted 250 replies posted 100 likes received

No, this is not a solution.
The problem reappears at the increase of 32,768 over the input signal.

0 Likes
lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

signal fillter

0 Likes
Anonymous
Not applicable

What happens if you increase the signal amplitude so that the mximum values goes above 33000?

0 Likes
lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

It leaves very bad signal

0 Likes
Anonymous
Not applicable

yes there are lessons to learn from this, what happens when an unsigned value is treated by a computation component as a signed value ?

   

If the signal stays in the range of the positive half of the numbers, then everything is ok, but you can only use half the signal range.

   

If the signal crosses the half range value, when the signed interpretation treats it as a maximum negative value, then the filter sees a sudden shift in signal from maximum positive to maximum negative, and there will be spikes and ringing.

   

Magnus

0 Likes
lock attach
Attachments are accessible only for community members.
feme_285141
Level 4
Level 4

decrease the sample filter in half compared to the ADC, and the image that happened shown. it  has  to do ???

0 Likes
feme_285141
Level 4
Level 4

how do I give the signal with sign ???

   

mode differntial????

0 Likes
Anonymous
Not applicable

It crosses the value 32768. Thats when it happens, as you clearly can see.

0 Likes
lock attach
Attachments are accessible only for community members.
EvPa_264126
Level 7
Level 7
500 replies posted 250 replies posted 100 likes received

Hello fernnando28. I often use the filters in my projects.
So I want to use your project as a starter.
I hope it will help me to configure filters.
I wonder what your project is very easy to organize a conclusion in USBUART.
It will not create problems?
In the example, "USBFS UART Code Example" the procedure is much more complicated.

0 Likes