cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

Hello All

   

Cypress has provided 001 kit to work with . Thanks to Cypress.

   

In the 001 kit i find something "wireless".

   

Can any one tell what is that device and its functionality.

   

Secondly where can i find the example project and work with it.(Cypress has provided 5 kits, if data transmissioin is poaaible among these will be great!!!!)

0 Likes
4 Replies
Anonymous
Not applicable

 I think it is for the CY3271-RFBOARD WIRELESS EXPANSION KIT, but not 100% sure.

0 Likes
Bob_Marlowe
Expert II

Yes, it is. Look here : http://www.cypress.com/?rID=17672

   

 

   

And there are some expansion kits as well.

   

Look in ths list : http://www.cypress.com/?app=search&searchType=advanced&keyword=&rtID=110&id=10&applicationID=0&l=0&s... 

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I was talking about wireless radio provided in the PSoC Cy8ckit-001.

   

But the kit you posted is different... and if you have any idea of how to use it or example projects please attacxh

0 Likes
Bob_Marlowe
Expert II

The Kits are NOT different, you can stick one of the boards just on to the interface of the -001 board. Together with the Kits I mentioned (they are PSoC1s) come a couple of example-projects up to a weather-station. The interesting points are: the boards transmit to a usb-interfaced master which talks to a program on your PC. There is a network-software for the boards which makes it really easy to have more than one of them connected via RF to the master.

   

When needing examples, download the installation files for the Kits and have a look at the examples.

   

 

   

Bob

0 Likes