Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
dari_292216
Level 2
Level 2
First like received First like given

 Is it Ok to use a 15V input into J4?  

   

I assume the regulator should tolerate it...  but just want to make sure.

   

Thanks!
--
Dario

 

0 Likes
3 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

J4 what ? What board ? -050 or -001 ?

   

 

   

If -050 regulator Vin rating is 18V, what you also have to be

   

concerned with is Pdiss, because if it hits an internal Tj of 150C

   

it will shutdown.

   

 

   

Regards, Dana.

0 Likes
dari_292216
Level 2
Level 2
First like received First like given

Sorry, yes, J4 on the CY8CKIT-050.
--
Dario

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

So to close the thread out what you care about is excess Pdiss in regulator.

   

 

   

For each 100 mA you use, with 15 Vin, and 5V out, thats 1W of Pdiss, which

   

is a lot of power for an SMT part w/no heatsink other than Cu pad area. So

   

if you plan on a lot of laods, like LEDs, you need to be aware of heat in the 5V

   

regulator.

   

 

   

Regards, Dana.

0 Likes