- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
How does Cypress explain the lack of PSOC3/5LP devices in the packages smaller than as big as they can have, i.e. QFN68 and TQFP100? The leadless packages such as QFN (3/5LP) or BGA (6+) are a guaranteed route to a disaster due to the lack of thermal strain relieve mechanism, while the gull wings have all the necessary springs, hence they are my only choice in high-rel/mid-rel applications. But then the only option on the table is TQFP100, which is way too big in many applications. I've just had to design PSOCs out of two projects just because there is no TQFP32 or 48 version of the chips. Microchip has many of their MCUs available in packages ranging from QFN down to DIP40 with the same chip inside. The same issue prevents me from ever considering PSOC6s in any of my designs, BTW.
Solved! Go to Solution.
- Labels:
-
PSoC 5LP


- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
We didn’t get too many requests for smaller packages for the PSOC 3/5LP devices in the past and hence did not create the same. Since this is an old product, we dont see Cypress creating new packages for these. You should be able to find smaller package options in PSoC 4 or new PSoC 6 families. Which package is of prime interest for you and your application? The QFN or DIP?