Warning - hold time violation found in a path from clock
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
I'm trying to build my project, but I get the following error which I can't seem to solve:

   

sta.M0019:  hold time violation found in a path from clock (cyBUS_clk) to clock (Pin_5(0)_ SYNC/OUT)

   

My project includes 1 SPI master and another (not related) SPI slave blocks.

   

I suspect the problem is due to the SPI slave which is controlled by an outside clock.

   

I've attached my project top design schematics.

   

 

   

Thanks in advance,

   

Igal Nudelman

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Welcome in the forum, Igal.

   

Your SPIS component's MOSI-pin (Pin_4) uses double sync at its input that is causing the warning. When set to none (no syncing) the warning passes.

   

 

   

Additionally: I would suggest to use an internal clock, since there is no need in your case for an external one on Pin_33. This clock is not controlling the bit-rate, it is for the component's internal updating of the states.

   

 

   

Bob

View solution in original post

0 Likes
8 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Welcome in the forum, Igal.

   

Your SPIS component's MOSI-pin (Pin_4) uses double sync at its input that is causing the warning. When set to none (no syncing) the warning passes.

   

 

   

Additionally: I would suggest to use an internal clock, since there is no need in your case for an external one on Pin_33. This clock is not controlling the bit-rate, it is for the component's internal updating of the states.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

 Thank you for your quick reply Bob.

   

 

   

Could you please tell me how to disable the syncing option of Pin 4? I didn't find it.

   

 

   

Best regards,

   

Igal

0 Likes
lock attach
Attachments are accessible only for community members.
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Configure the pin as attached picture

   

 

   

Bob

Anonymous
Not applicable

 It worked!

   

 

   

Thanks a lot for the answers and the warm welcome 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Fine that I could help you. You are always welcome.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Some thoughts -

   

 

   

1) You do not have hysterisis enabled on the comparators, if your

   

compare signal is noisy you might want to consider that.

   

 

   

2) You used up all your comparator blocks, if you needed more consider

   

using the scanning comparator block, and if the references need to be channel

   

specific use a mux for that as well. Or use the SAR, its capable of 1 MSPS, and I

   

noticed your comparators set for slow speed, eg. 200 nS response time. It also

   

gives you much more control over equivalent reference trip points.

   

 

   

   

 

   

3) You used IDAC followed by TIA, I assume to get a VDAC ? You can always terminate

   

the IDAC with an R to get a VDAC. Disadvantage is its not buffered, however if its destination

   

is hi Z then would work. Even if it was R based load of known value you could use that R in

   

the determination of IDAC R.

   

 

   

4) The IDAC uses a ref of Vdd /2, so you limit your range to Vdd / 2, is that what you wanted,

   

or would just Vdda as a ref, which increases range, be more useful.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Hello Dana,

   

Thank you for your suggestions.

   

1. I might add hystersis, not sure about it at the moment.

   

2. I know I used all my comperators, and it doesn't look like I'll need more. I don't think I can use your suggestion for scanning comperator block because I need different values (and the ability to control them) to be compared to.

   

In addition to that, I need this process to be fast (<6uS) and the SAR won't give me this speed (it's 1MSPS for 1 bit).

   

3. You're correct. I used IDAC to get VDAC. When I use Vdd/2 reference and I change the current direction (sink or source) I can get 9bit VDAC for 5V instead of the VDAC that PSOC offers that's set to limit of only 4V and 8bit.

   

The TIA is for buffering and some filtering as well.

   

 

   

I hope my answers will give you new ideas for your future projects.

   

Best regards,

   

Igal

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

2. I know I used all my comperators, and it doesn't look like I'll need more. I don't think I can use your suggestion for scanning comperator block because I need different values (and the ability to control them) to be compared to.

   

 

   

Thats code, you have infinite flexibility for comparisons to a reference V of your

   

choosing, to the A/D value measured. You can even make it adpative.

   

 

   

In addition to that, I need this process to be fast (<6uS) and the SAR won't give me this speed (it's 1MSPS for 1 bit).

   

 

   

SAR yields a 12 bit conversion in 1 uS. However to your point you do the conversion

   

and then execute some code, not much I would add. If you use SAR at 10 bits it

   

will do 1.125 MSPS, at 8 bits even faster, 1.285 MSPS.

   

 

   

The suggestions are simply in case you run out of HW resources.

   

 

   

Regards, Dana.

0 Likes