- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm trying to build my project, but I get the following error which I can't seem to solve:
sta.M0019: hold time violation found in a path from clock (cyBUS_clk) to clock (Pin_5(0)_ SYNC/OUT)
My project includes 1 SPI master and another (not related) SPI slave blocks.
I suspect the problem is due to the SPI slave which is controlled by an outside clock.
I've attached my project top design schematics.
Thanks in advance,
Igal Nudelman
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum, Igal.
Your SPIS component's MOSI-pin (Pin_4) uses double sync at its input that is causing the warning. When set to none (no syncing) the warning passes.
Additionally: I would suggest to use an internal clock, since there is no need in your case for an external one on Pin_33. This clock is not controlling the bit-rate, it is for the component's internal updating of the states.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum, Igal.
Your SPIS component's MOSI-pin (Pin_4) uses double sync at its input that is causing the warning. When set to none (no syncing) the warning passes.
Additionally: I would suggest to use an internal clock, since there is no need in your case for an external one on Pin_33. This clock is not controlling the bit-rate, it is for the component's internal updating of the states.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you for your quick reply Bob.
Could you please tell me how to disable the syncing option of Pin 4? I didn't find it.
Best regards,
Igal
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
It worked!
Thanks a lot for the answers and the warm welcome
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Fine that I could help you. You are always welcome.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Some thoughts -
1) You do not have hysterisis enabled on the comparators, if your
compare signal is noisy you might want to consider that.
2) You used up all your comparator blocks, if you needed more consider
using the scanning comparator block, and if the references need to be channel
specific use a mux for that as well. Or use the SAR, its capable of 1 MSPS, and I
noticed your comparators set for slow speed, eg. 200 nS response time. It also
gives you much more control over equivalent reference trip points.
3) You used IDAC followed by TIA, I assume to get a VDAC ? You can always terminate
the IDAC with an R to get a VDAC. Disadvantage is its not buffered, however if its destination
is hi Z then would work. Even if it was R based load of known value you could use that R in
the determination of IDAC R.
4) The IDAC uses a ref of Vdd /2, so you limit your range to Vdd / 2, is that what you wanted,
or would just Vdda as a ref, which increases range, be more useful.
Regards, Dana.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Dana,
Thank you for your suggestions.
1. I might add hystersis, not sure about it at the moment.
2. I know I used all my comperators, and it doesn't look like I'll need more. I don't think I can use your suggestion for scanning comperator block because I need different values (and the ability to control them) to be compared to.
In addition to that, I need this process to be fast (<6uS) and the SAR won't give me this speed (it's 1MSPS for 1 bit).
3. You're correct. I used IDAC to get VDAC. When I use Vdd/2 reference and I change the current direction (sink or source) I can get 9bit VDAC for 5V instead of the VDAC that PSOC offers that's set to limit of only 4V and 8bit.
The TIA is for buffering and some filtering as well.
I hope my answers will give you new ideas for your future projects.
Best regards,
Igal
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
2. I know I used all my comperators, and it doesn't look like I'll need more. I don't think I can use your suggestion for scanning comperator block because I need different values (and the ability to control them) to be compared to.
Thats code, you have infinite flexibility for comparisons to a reference V of your
choosing, to the A/D value measured. You can even make it adpative.
In addition to that, I need this process to be fast (<6uS) and the SAR won't give me this speed (it's 1MSPS for 1 bit).
SAR yields a 12 bit conversion in 1 uS. However to your point you do the conversion
and then execute some code, not much I would add. If you use SAR at 10 bits it
will do 1.125 MSPS, at 8 bits even faster, 1.285 MSPS.
The suggestions are simply in case you run out of HW resources.
Regards, Dana.