- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
For the ones interested, I created a Visual Studio Code setup for PSoC5.
The setup makes use of PSoC Creator which is needed for the (one time) configuration of the schematic / system / UDB part (and needs Windows to run of course). Once the configuration is done, coding and debugging can be done with Visual Studio Code (which can run on the platform of your choice). The advantage as well is that the PSoC Creator is 'embedded'. Changing the schematic / system / UDB part can be done in the 'embedded PSoC Creator project' without having to export / copy the project.
The result is a very fast, transparent, smooth and stable IDE for use with PSoC5.
https://github.com/RolfNoot/PSoC5_VS_Creator
When there's enough interest I can provide PSoC3 and PSoC4 setups as well.
Edit: Added the post build executable C# project sources.
Solved! Go to Solution.
- Labels:
-
PSoC1 MCU
-
PSoC3 MCU
-
PSOC5 LP MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi ,
Thank you @Rolf_Nooteboom for taking the time for creating and contributing the Visual Studio Code Setup for PSoC Creator. We appreciate this contribution :).
Locking this thread due to inactivity for long time, you can continue the discussion on the topic by opening a new thread with reference to the locked one. The continuous discussion in an inactive thread may mostly be unattended by community users.
Thanks and Regards,
Alen Austin